Wiki

This version (15 Sep 2017 11:58) was approved by Venkatesan Krishnamoorthy.The Previously approved version (15 Sep 2017 11:56) is available.Diff

Algorithm Version History

Click here to return to the Using SigmaStudio page

When any modification is done for fixing a bug/ improving some features algorithms are made obsolete in the SigmaStudio. Please refer the Obsoleted Algorithms section for more details. Sometimes customers needed to use the older version of the algorithm. This can be done using Algorithm Version History table. But this feature is supported only for the algorithms made obsolete from SigmaStudio Release 3.15

Usage

To see the version history of a particular algorithm. Right click on the module and select algorithm version history.

Algorithm Version History table will list the algorithms current version in Green color. User can click the 'Revert to this' button to revert to any particular version.

resources/tools-software/sigmastudio/usingsigmastudio/algorithmversion.txt · Last modified: 15 Sep 2017 11:58 by Venkatesan Krishnamoorthy