This schematic shows a simple way of smoothly switching (crossfading) from one signal to the other (here 500 Hz and 2kHz). It uses these blocks: DC Input control entry, two Tone (Lookup/Sine), Crossfade (Data-Controlled), and Output.
This schematic shows a simple way of multiplexing two sources and then demultiplexing the signals to two outputs. Two Tone (Lookup/Sine) blocks feed an Index-Selectable Multiplexer, with the switching between them controlled by a DC Input. The output goes to an Index-Selectable Demultiplexer, whose behavior is controlled by a second DC Input Entry to feed two Outputs.
This schematic uses Mono Switch 1xN and Mono Switch Nx1 flanking a General (2nd-Order) Filter grown by 2. The filter frequency response choice is highpass and the highpassed signal is routed to the output. Tone (Lookup/Sine), Probe, Stimuli and Output blocks complete the signal flow.
Below is the frequency response of the HP filter.
This schematic shows a simple way of multiplexing two sources using two State-Variable filters, Stereo Switch Nx2, Input and Output blocks. The filters' high-pass outputs are selected and routed to the output blocks.