Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Last revisionBoth sides next revision
resources:tools-software:sigmastudio:tutorials:microcontroller [03 Jan 2021 21:46] – fix links Robin Getzresources:tools-software:sigmastudio:tutorials:microcontroller [10 Feb 2021 14:30] – fix links Robin Getz
Line 65: Line 65:
  
 ==== ADAU1761 ==== ==== ADAU1761 ====
-The ADAU1761 (referred to as Sigma200) has a similar pinout to the ADAU1701, although I2C pullup resistors are already in place on the board. The evaluation board schematic is available [[resources:tools-https://www.analog.com/media/en/technical-documentation/evaluation-documentation/EVAL-ADAU1761Z.pdf|here]].+The ADAU1761 (referred to as Sigma200) has a similar pinout to the ADAU1701, although I2C pullup resistors are already in place on the board. The evaluation board schematic is available [[adi>media/en/technical-documentation/evaluation-documentation/EVAL-ADAU1761Z.pdf|here]].
  
 EVAL-ADAU1761Z also allows Pin 4 of the USBi connector to power the DSP. Again, ensure that your system consumes <500mA from a USB port. EVAL-ADAU1761Z also allows Pin 4 of the USBi connector to power the DSP. Again, ensure that your system consumes <500mA from a USB port.
resources/tools-software/sigmastudio/tutorials/microcontroller.txt · Last modified: 05 May 2021 13:56 by Joshua Berlin