This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:tools-software:sigmastudio:tutorials:adav801srcexample [30 Jul 2012 21:24] William Jahn Approved |
resources:tools-software:sigmastudio:tutorials:adav801srcexample [03 Jan 2021 21:46] Robin Getz fix links |
||
---|---|---|---|
Line 16: | Line 16: | ||
\\ | \\ | ||
- | <note tip>Please refer to the following supporting documents if any further clarification is needed throughout this example | + | <WRAP tip>Please refer to the following supporting documents if any further clarification is needed throughout this example |
- | * [[http://www.analog.com/static/imported-files/data_sheets/ADAV801.pdf|ADAV801 datasheet]] | + | * [[adi>static/imported-files/data_sheets/ADAV801.pdf|ADAV801 datasheet]] |
- | * [[http://www.analog.com/static/imported-files/application_notes/60376866819334AN749_0.pdf|Application Note AN-749]] | + | * [[adi>static/imported-files/application_notes/60376866819334AN749_0.pdf|Application Note AN-749]] |
- | </note> | + | </WRAP> |