This is an old revision of the document!
Click here to return to the Volume Controls section.
When enabled, the Mute block “mutes” the input signal so that their is no output (a 0.0 value DC signal). This is useful when powering up or down and when switching program flow. | ![]() |
To Enable/Disable the mute:
Click the check box, the signal is mutes when the box is checked.
The mute block include's Slew and Non-Slew type algorithms. Slew algorithms will smoothly transition the gain to zero, eliminating any click or pops, but require more system resources.
Algorithms:
This block supports both Grow Algorithm (adds additional inputs and outputs) and Add Algorithm (adds an independent mute algorithm plus associated inputs and outputs).