Click here to return to the System page
The Hierarchy output block is used to create signal outputs from a Schematic Hierarchy Tab. Hierarchy Boards are helpful for large schematic designs and for organizing design components.
For more information about Hierarchy Boards, see the Hierarchy Boards topic.
To create a Hierarchy Output:
Note: To see determine which Hierarchy output block belongs to a Hierarchy board output pin, hover the mouse pointer above the Hierarchy board pin and the output block's name will be displayed in the tool-tip (as in the image above).
See the Hierarchy Board System Example for a sample hierarchy board design.