This is an old revision of the document!
Click here to return to the Sources section.
This module can be used to read PCM/WAV files from internal memory of ADAU145x. This module also provides playback controls as Play/Pause, Stop and Loopback.This module also can perform pitch shifting while playing the file.
The following list shows the various audio files supported by this module.
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: WavPlayer OutPut | decimal - audio | Audio Sample |
The module currently does not support grow/add functionality.
Click on the image to open the Wav Player Properties Window.
GUI Control Name | Default Value | Range | Function Description |
---|---|---|---|
Audio File Format | Audio Sample in 8.24 | Wav without header (PCM)/Audio Sample in 8.24 format | Selection of audio file format |
Bits Per Sample | 32 | 8/16/24/32 | Bits per sample in the audio file Load. |
Sample to Start | 0 | 0 - number of samples in file | To allow phase shift. |
File Type | ASCII | ASCII/Binary | To select text file or PCM file. |
Note: The size of the file shall not exceed the (Maximum DM0 Memory(20kb) - Available DM0 Memory).
Any change in these configuration parameters requires a recompilation.
GUI Control Name | Compiler Name | Function Description |
---|---|---|
ForwardPlay | WavPlayerInternalAlg1ForwardPlay | To Play or Pause the Audio |
Loopback | WavPlayerInternalAlg1Loopback | To Enable/Disable Loopback |
PitchScalingFactor | WavPlayerInternalAlg1PitchScalingFactor | To provide pitch shifting |
PitchScalingCounter | WavPlayerInternalAlg1PitchScalingCounter | To provide phase shift |
Here,