This shows you the differences between two versions of the page.
Previous revision | |||
— | resources:tools-software:sigmastudio:toolbox:sources:vcowithquadratureoutputs [02 Aug 2012 21:04] (current) – Added toolbox hierarchy Brett Gildersleeve | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== VCO with Quadrature Outputs ====== | ||
+ | [[: | ||
+ | |||
+ | |The voltage-controlled oscillator block, typically used for modulation applications, | ||
+ | \\ \\ | ||
+ | The input value may be from zero to one (5.23 format), and the VCO linearly interpolates its derived value into an output frequency from 0 Hz (0.0 input) to fs/2 (1.0 input). Fs is the sampling frequency. | ||
+ | \\ \\ | ||
+ | If the input applied is greater than 1, the derived output value will fold back to frequencies below fs/2. | ||
+ | \\ \\ | ||
+ | To change the source' | ||
+ | \\ \\ | ||
+ | This cell can be found in the Voltage Controlled subfolder in the Sources section of the toolbox. | ||
+ | \\ | ||
+ | {{: | ||
+ | \\ |