Click here to return to the Sources section.
The input value may be from zero to one (5.23 format), and the VCO linearly interpolates its derived value into an output frequency from 0 Hz (0.0 input) to fs/2 (1.0 input). Fs is the sampling frequency.
If the input applied is greater than 1, the derived output value will fold back to frequencies below fs/2.
To change the source's Sampling Rate, Right-click in the block and select Set Sampling Rate, which will open the Sampling Rate window (default is 44.1 kHz).
This cell can be found in the Voltage Controlled subfolder in the Sources section of the toolbox.