Wiki

This version is outdated by a newer approved version.DiffThis version (02 Aug 2012 16:27) was approved by Brett Gildersleeve.

This is an old revision of the document!


Voltage Controlled Oscillator Reset Phase

The voltage-controlled oscillator block (reset phase), typically used for modulation applications, takes a control input signal (second red pin) and outputs a sine tone at a particular frequency on the blue pin. It also has a control pin that resets the phase of the output signal.vco_004.jpg



The input value may be from zero to one (5.23 format), and the VCO linearly interpolates its derived value into an output frequency from 0 Hz (0.0 input) to fs/2 (1.0 input). Fs is the sampling frequency.

If the input applied is greater than 1, the derived output value will fold back to frequencies below fs/2.

To change the source's Sampling Rate, Right-click in the block and select Set Sampling Rate, which will open the Sampling Rate window (default is 44.1 kHz).

resources/tools-software/sigmastudio/toolbox/sources/vcoresetphase.1343917653.txt.gz · Last modified: 02 Aug 2012 16:27 (external edit)