Wiki

This version (02 Aug 2012 20:58) was approved by Brett Gildersleeve.The Previously approved version (02 Aug 2012 16:27) is available.Diff

Voltage Controlled Oscillator Reset Phase

Click here to return to the Sources section.

The voltage-controlled oscillator block (reset phase), typically used for modulation applications, takes a control input signal (second red pin) and outputs a sine tone at a particular frequency on the blue pin. It also has a control pin that resets the phase of the output signal.vco_004.jpg



The input value may be from zero to one (5.23 format), and the VCO linearly interpolates its derived value into an output frequency from 0 Hz (0.0 input) to fs/2 (1.0 input). Fs is the sampling frequency.

If the input applied is greater than 1, the derived output value will fold back to frequencies below fs/2.

To change the source's Sampling Rate, Right-click in the block and select Set Sampling Rate, which will open the Sampling Rate window (default is 44.1 kHz).

resources/tools-software/sigmastudio/toolbox/sources/vcoresetphase.txt · Last modified: 02 Aug 2012 20:58 by Brett Gildersleeve