Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:tools-software:sigmastudio:toolbox:sources:squarewavewithphaseandgain [20 Jan 2016 10:22] Venkatesan Krishnamoorthyresources:tools-software:sigmastudio:toolbox:sources:squarewavewithphaseandgain [20 Jan 2016 10:26] (current) Venkatesan Krishnamoorthy
Line 19: Line 19:
 |Initial Phase|0|0 to 360|Initial Phase of the square wave.| |Initial Phase|0|0 to 360|Initial Phase of the square wave.|
 |Gain|0|-144 to 42 dB| The gain to be multiplied on the square wave| |Gain|0|-144 to 42 dB| The gain to be multiplied on the square wave|
 +
 +<WRAP center round info 60%>
 +Note: The square wave is digitally generated and is **non-bandlimited**.  This waveform is suitable for use as an internal control signal, but will produce aliasing distortion if used directly for audio output. If this configuration is desired, it is recommended that you apply a low-pass filter to the block's output before routing the signal to hardware outputs.
 +</WRAP>
  
resources/tools-software/sigmastudio/toolbox/sources/squarewavewithphaseandgain.txt · Last modified: 20 Jan 2016 10:26 by Venkatesan Krishnamoorthy