Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:tools-software:sigmastudio:toolbox:sources:sawtoothwavewithphaseandgain [06 Sep 2016 13:37] Venkatesan Krishnamoorthyresources:tools-software:sigmastudio:toolbox:sources:sawtoothwavewithphaseandgain [06 Sep 2016 13:37] (current) Venkatesan Krishnamoorthy
Line 9: Line 9:
 To change the source's Sampling Rate, Right-click in the block and select Set Sampling Rate, which will open the Sampling Rate window (default is 44.1 kHz). To change the source's Sampling Rate, Right-click in the block and select Set Sampling Rate, which will open the Sampling Rate window (default is 44.1 kHz).
  
-===GUI Control===+=====GUI Control=====
 ^GUI Control Name^Default Value^Range^Function Description^ ^GUI Control Name^Default Value^Range^Function Description^
 |on/off|off|on/off|Turns the output of the cell on or off. When the output is off, the output pin will output a constant value of 0.| |on/off|off|on/off|Turns the output of the cell on or off. When the output is off, the output pin will output a constant value of 0.|
Line 16: Line 16:
 |Gain|0|-144 to 42 dB / -134 to 24 db| The gain to be multiplied on the sawtooth wave| |Gain|0|-144 to 42 dB / -134 to 24 db| The gain to be multiplied on the sawtooth wave|
  
-=== Growth ===+===== Growth =====
 This module can be grown to support multiple phase/gain values for a single sawtooth wave.  This module can be grown to support multiple phase/gain values for a single sawtooth wave. 
 {{ :resources:tools-software:sigmastudio:toolbox:sources:sawto.jpg?nolink |}} {{ :resources:tools-software:sigmastudio:toolbox:sources:sawto.jpg?nolink |}}
resources/tools-software/sigmastudio/toolbox/sources/sawtoothwavewithphaseandgain.txt · Last modified: 06 Sep 2016 13:37 by Venkatesan Krishnamoorthy