Click here to return to the Sources section.
To Do: This page currently shows information for the Chime Freq-Gain algorithm. It needs to be changed to show the Chime Frequency algorithm.
The Chime Freq-Gain algorithm plays back a chime sound with programmable, independent frequency and gain envelopes. | ![]() |
There are two versions of the algorithm available:
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Chime Activate | int - control | Switch used to activate chime |
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Audio Output | decimal - audio | Chime Audio Output |
GUI Control Name | Default Value | Range | Function Description |
---|---|---|---|
Maximum Time (ms) | 1004 | 10 to 4400 | Determines the length of the x axis in the envelope control window |
Envelope Control | n/a | n/a | Allows the frequency and gain curves to be manually adjusted. Double-clicking on the graph creates a new point. Right clicking on the graph allows points to be removed. The graph can be zoomed using the zoom icons in the upper left corner. |
Frequency (Hz) | n/a | 20 to 20000 | Controls the frequency coordinate of the corresponding point on the envelope |
Time (ms) | n/a | 0 to max | Controls the time coordinate of the corresponding point on the envelope |
Gain (dB) | n/a | -120 to +24 | Controls the gain coordinate of the corresponding point on the envelope |
GUI Name | Compiler Name | Function Description |
---|---|---|
Envelope Control | Optimized2ChimeAlgWGainGUI1numberofpoints | Number of points in the timing table |
Envelope Control | Optimized2ChimeAlgWGainGUI1table | First point in the timing table |
Envelope Control | Optimized2ChimeAlgWGainGUI1table_autoincremented | Timing table values (continued) |
… | … | … |
Envelope Control | Optimized2ChimeAlgWGainGUI1numberofgainpoints | Number of points in the gain table |
Envelope ControlOptimized2ChimeAlgWGainGUI1gaintable | First point in the gain table | |
Envelope Control | Optimized2ChimeAlgWGainGUI1gaintable_autoincremented | Gain table values (continued) |
… | … | … |
Envelope Control | Optimized2ChimeAlgWGainGUI1freqincrement | Increment value for frequency table |
Envelope Control | Optimized2ChimeAlgWGainGUI1freqincrement_autoincremented | Frequency table values (continued) |
… | … | … |
Envelope Control | Optimized2ChimeAlgWGainGUI1startfreq | Beginning frequency of the chime |
Envelope Control | Optimized2ChimeAlgWGainGUI1lowestfreq | Lowest frequency in the chime’s frequency envelope |
Envelope Control | Optimized2ChimeAlgWGainGUI1gainincrementtable | First point in the gain increment table |
Envelope Control | Optimized2ChimeAlgWGainGUI1gainincrementtable_autoincremented | Gain increment table values (continued) |
… | … | … |
Envelope Control | Optimized2ChimeAlgWGainGUI1startgain | Starting gain value of the gain envelope |
Envelope Control | Optimized2ChimeAlgWGainGUI1lowestgain | Lowest gain value in the gain envelope |
Envelope Control | Optimized2ChimeAlgWGainGUI1mask | Mask |
The chime algorithm has fully programmable frequency and gain envelopes. The envelopes are accessible by clicking the cell’s icon.
The length of the chime is controlled by the Maximum Time control, which is set in milliseconds.
The envelope control window has two tabs: Frequency and Gain. The Frequency envelope is displayed in blue, and the Gain envelope is displayed in red. Points on the curve can be moved by click-dragging. New points can be added by double-clicking. Points can be removed by right-clicking and selecting “remove point.” In this case, the point closest to the mouse cursor will be removed. Each envelope must have at least 3 points. Point values can be fine-tuned using the text input boxes on the right side of the envelope control window.
When the control input goes to 1, the chime begins. When the control input goes to 0, the chime output stops, regardless of whether the envelope has completed or not.
In the case of the Chime Freq – Gain Continuous Play algorithm, the envelope will loop continuously until the control input goes to 0.
The example below shows the chime algorithm’s input and output signals using the gain envelope shown above.
The example below has the input going to zero before the envelope has completed. The output will immediately go to zero.
The following schematic image shows the Chime Freq-Gain cell being used with a 28.0 switch and being output to a DAC. The schematic below uses the Switch, Chime Freq-Gain, and Output cells.
Toolbox Path | Sources – Chime – Modulated Frequency and Gain |
Cores Supported | AD1940 ADAU144x ADAU176x ADAU178x |
“Grow Algorithm” Supported | no |
“Add Algorithm” Supported | no |
Subroutine/Loop Based | no |
Program RAM | 96 |
Data RAM | 21 |
Parameter RAM | 31 |