Wiki

This version (25 Jul 2012 21:09) was approved by Brett Gildersleeve.

SigmaStudio Muxes/Demuxes Algorithm Resource Summary

The information here is preliminary.

Click here to return to the SigmaStudio Algorithm Resource Summary section.

CategoryAlgorithmExecuted InstructionsProgram RAMDATA RamParameter RAMDescriptionProcessors
State MachineState Machine151522Outputs the input signal from the green pin, if and only if the control signal level (orange pin) falls within the range specified in the numerical spin controls (>) and (<).ADAU144x, ADAU176x, ADAU1781
State MachineState Machine (Grow)151512Adds another channel for an State Machine algorithm to the block.ADAU144x, ADAU176x, ADAU1781
DemultiplexersMonoIndex Selectable Demutiplexer121240Lets you route an input to one of two selectable output pins.ADAU144x, ADAU176x, ADAU1781
DemultiplexersMonoIndex Selectable Demutiplexer (Grow)4440Adds another output to the block.ADAU144x, ADAU176x, ADAU1781
DemultiplexersStereoIndex Selectable Demutiplexer242480Lets you route an input to one of two selectable output pins.ADAU144x, ADAU176x, ADAU1781
DemultiplexersStereoIndex Selectable Demutiplexer (Grow)8840Adds another output to the block.ADAU144x, ADAU176x, ADAU1781
DemultiplexersNo SlewMono Switch 1xn4422Routes an input signal to one of many possible outputs. The strip of radio buttons is used to select an output (each radio button corresponds to a coefficient RAM parameter).ADAU144x, ADAU176x, ADAU1781
DemultiplexersNo SlewMono Switch 1xn (Grow)2211Adds another output and corresponding switch to the block.ADAU144x, ADAU176x, ADAU1781
DemultiplexersNo SlewStereo Switch 2xn8842Route a stereo input to one of several possible stereo outputs with this block, using the strip of radio button pairs to select which output.ADAU144x, ADAU176x, ADAU1781
DemultiplexersNo SlewStereo Switch 2xn (Grow)4421Adds another two outputs (stereo pair) and corresponding switch to the block.ADAU144x, ADAU176x, ADAU1781
DemultiplexersClickless SW SlewMono Switch 1xn2222112Routes an input signal to one of many possible outputs, the strip of radio buttons is used to select an output (each radio button corresponds to a coefficient RAM parameter).ADAU144x, ADAU176x, ADAU1781
DemultiplexersClickless SW SlewMono Switch 1xn (Grow)111151Adds another output and corresponding switch to the block.ADAU144x, ADAU176x, ADAU1781
DemultiplexersClickless SW SlewStereo Switch 2xn2626132Route a stereo input to one of several possible stereo outputs with this block, using the strip of radio button pairs to select which output.ADAU144x, ADAU176x, ADAU1781
DemultiplexersClickless SW SlewStereo Switch 2xn (Grow)131361Adds another two outputs (stereo pair) and corresponding switch to the block.ADAU144x, ADAU176x, ADAU1781
MultiplexerMonoIndex Selectable Multiplexer101030Routes the signal from either of its two input pins, based on the control signal input index value from the Index Lookup Table, RMS Table or DC Input.ADAU144x, ADAU176x, ADAU1781
MultiplexerMonoIndex Selectable Multiplexer (Grow)2210Adds another input to the multiplexer.ADAU144x, ADAU176x, ADAU1781
MultiplexerStereoIndex Selectable Multiplexer181870Routes the signal from either of its two input pins, based on the control signal input index value from the Index Lookup Table, RMS Table or DC Input.ADAU144x, ADAU176x, ADAU1781
MultiplexerStereoIndex Selectable Multiplexer (Grow)4420Adds another two inputs (stereo pair) to the multiplexer.ADAU144x, ADAU176x, ADAU1781
MultiplexerIndex Selectable Slewing Mux6060192Routes any one of its inputs, based on the index value from the Index Lookup Table, RMS Table or DC input, letting you ramp the source level up and down without any clicking noises when switching inputs.ADAU144x, ADAU176x, ADAU1781
MultiplexerIndex Selectable Slewing Mux (Grow)2210Adds another input to the multiplexer.ADAU144x, ADAU176x, ADAU1781
MultiplexerNo SlewMono Switch Nx13312Routes one of many possible input signals to the output. The strip of radio buttons is used to select the input signal (each radio button corresponds to a coefficient RAM parameter).ADAU144x, ADAU176x, ADAU1781
MultiplexerNo SlewMono Switch Nx1 (Grow)1101Adds another input and corresponding switch to the block.ADAU144x, ADAU176x, ADAU1781
MultiplexerNo SlewStereo Switch Nx26622Select between or among sets of stereo inputs and send one set to one of the (2-channel) outputs.ADAU144x, ADAU176x, ADAU1781
MultiplexerNo SlewStereo Switch Nx2 (Grow)2211Adds another two inputs (stereo pair) and corresponding switch to the block.ADAU144x, ADAU176x, ADAU1781
MultiplexerNo SlewMulti CH Switch Nx4121242Select among sets of 4 inputs and send one set to one of the (4-channel) outputs.ADAU144x, ADAU176x, ADAU1781
MultiplexerNo SlewMulti CH Switch Nx4 (Grow)4401Adds another 4 inputs as well as a corresponding switch to the block.ADAU144x, ADAU176x, ADAU1781
MultiplexerNo SlewMulti CH Switch Nx6181862Select among sets of 6 inputs and send one set to one of the (6-channel) outputs.ADAU144x, ADAU176x, ADAU1781
MultiplexerNo SlewMulti CH Switch Nx6 (Grow)6601Adds another 6 inputs as well as a corresponding switch to the block.ADAU144x, ADAU176x, ADAU1781
MultiplexerNo SlewMulti CH Switch Nx8242482Select among sets of 8 inputs and send one set to one of the (8-channel) outputs.ADAU144x, ADAU176x, ADAU1781
MultiplexerNo SlewMulti CH Switch Nx8 (Grow)8801Adds another 8 inputs as well as a corresponding switch to the block.ADAU144x, ADAU176x, ADAU1781
MultiplexerClickless SW SlewMono Switch Nx16060191Routes one of many possible input signals to the output. The strip of radio buttons is used to select the input signal (each radio button corresponds to a coefficient RAM parameter).ADAU144x, ADAU176x, ADAU1781
MultiplexerClickless SW SlewMono Switch Nx1 (Grow)2210Adds another input and corresponding switch to the block.ADAU144x, ADAU176x, ADAU1781
MultiplexerClickless SW SlewStereo Switch Nx26969221Select between or among sets of stereo inputs and send one set to one of the (2-channel) outputs.ADAU144x, ADAU176x, ADAU1781
MultiplexerClickless SW SlewStereo Switch Nx2 (Grow)7373241Adds another two inputs (stereo pair) and corresponding switch to the block.ADAU144x, ADAU176x, ADAU1781
Cross FadeCrossfade (Data Controlled)161671Creates a smooth transition between two input signals: the volume of one signal is decreased while the other input signal level increases, creating a gradual switch (cross-fade) between the inputs.ADAU144x, ADAU176x, ADAU1781
Cross FadeCrossfade (Data Controlled) (Grow)5510Adds another two inputs to the block.ADAU144x, ADAU176x, ADAU1781
resources/tools-software/sigmastudio/toolbox/muxesdemuxesresourcetable.txt · Last modified: 25 Jul 2012 21:09 by Brett Gildersleeve