The Cross Mux block allows route an input to one of selected output pins. The output for each input is selected based on the numeric value on the control.
Name | ADSP-214xx | ADSP-215xx/SC5xx | ADAU145x/146x |
---|---|---|---|
Cross Mux | Block | Block | NA |
Name | Type | Description |
---|---|---|
InputX | Audio | Input Channel X |
Name | Type | Description |
---|---|---|
OutputX | Audio | Output Channel X |
Note:
GUI Parameter | Default Value | Range | Function Description |
---|---|---|---|
Index_ChannelX | 0 | 0 to 100 | Selects the output channel to route the input |
NumInputs | 1 | 1 to 23 | Number of input channels. Change in this value requires re-compilation |
NumOuputs | 1 | 1 to 23 | Number of output channels. Change in this value requires re-compilation |
Note:
Parameter Name | Description | ADSP-214xx/SC5xx/215xx | ADAU145x/146x |
---|---|---|---|
Index_ChannelX | Selects the output channel to route the input | Float | NA |
Note: