This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:sigmastudio:toolbox:multirateprocessing:upsampling [12 May 2017 14:23] – Suhasini Raghuram | resources:tools-software:sigmastudio:toolbox:multirateprocessing:upsampling [04 Jan 2021 06:21] (current) – Updated UpSample Image Sanjeeva Reddy | ||
---|---|---|---|
Line 6: | Line 6: | ||
\\ | \\ | ||
\\ | \\ | ||
- | {{ : | + | {{ : |
\\ | \\ | ||
Line 27: | Line 27: | ||
^GUI Control Name^Default Value^Range^Function Description^ | ^GUI Control Name^Default Value^Range^Function Description^ | ||
|Upsample Factor|2| 2, | |Upsample Factor|2| 2, | ||
- | |LPF|Checked|Checked/ | ||
The upsampler can either insert zeros or repeat the previous sample(Zero Order Hold) during upsampling. This can be configured in the contex menu. | The upsampler can either insert zeros or repeat the previous sample(Zero Order Hold) during upsampling. This can be configured in the contex menu. |