This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:tools-software:sigmastudio:toolbox:multirateprocessing:upsampling [12 May 2017 14:23] Suhasini Raghuram |
resources:tools-software:sigmastudio:toolbox:multirateprocessing:upsampling [04 Jan 2021 06:21] Sanjeeva Reddy Updated UpSample Image |
||
---|---|---|---|
Line 6: | Line 6: | ||
\\ | \\ | ||
\\ | \\ | ||
- | {{ :resources:tools-software:sigmastudio:toolbox:multirateprocessing:upsampling.png?nolink | | + | {{ :resources:tools-software:sigmastudio:toolbox:multirateprocessing:upsampling4p6.png?nolink |}} |
\\ | \\ | ||
Line 27: | Line 27: | ||
^GUI Control Name^Default Value^Range^Function Description^ | ^GUI Control Name^Default Value^Range^Function Description^ | ||
|Upsample Factor|2| 2,3,4,6,8,16 |The factor at with the input sample rate will be multipiled| | |Upsample Factor|2| 2,3,4,6,8,16 |The factor at with the input sample rate will be multipiled| | ||
- | |LPF|Checked|Checked/Unchecked|If checked, a low pass filter will be applied after upsampling the signal| | ||
The upsampler can either insert zeros or repeat the previous sample(Zero Order Hold) during upsampling. This can be configured in the contex menu. | The upsampler can either insert zeros or repeat the previous sample(Zero Order Hold) during upsampling. This can be configured in the contex menu. |