Wiki

This version (04 Jan 2021 06:21) was approved by Sanjeeva Reddy.The Previously approved version (12 May 2017 14:23) is available.Diff

Up Sampling

Click here to return to the Multi-rate processing section.

The Up sampling module is mainly used to get the input samples to a higher sampling rates after processing the audio at lower sampling rates.For example the bass of the audio can be processed at lower sampling rates and then taken to the higher sampling rates.


Input Pins

NameFormat [int/dec] - [control/audio]Function Description
Pin 0: Inputdecimal- audioInput Signal to be up-sampled.


Output Pins

NameFormat [int/dec] - [control/audio]Function Description
Pin 0: Outputdecimal - audioUpsampled Output


Grow Algorithm

The module can be grown upto 8 channels. All the input signals are upsampled by the same upsample rate.

Configurations

The upsample factor can be changed by combo box.

GUI Control NameDefault ValueRangeFunction Description
Upsample Factor2 2,3,4,6,8,16 The factor at with the input sample rate will be multipiled

The upsampler can either insert zeros or repeat the previous sample(Zero Order Hold) during upsampling. This can be configured in the contex menu.

Change in the 'Insertion Type' , 'Upsample Factor' or 'LPF' needs a recompilation of the schematic.

DSP Parameter Information

None

Supported ICs

  1. ADAU145x
resources/tools-software/sigmastudio/toolbox/multirateprocessing/upsampling.txt · Last modified: 04 Jan 2021 06:21 by Sanjeeva Reddy