This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:statemachine [03 Aug 2012 17:14] Brett Gildersleeve Created |
resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:statemachine [03 Aug 2012 17:36] Brett Gildersleeve Added link |
||
---|---|---|---|
Line 1: | Line 1: | ||
====== State Machine ====== | ====== State Machine ====== | ||
- | This block outputs the input signal from the green pin, if and only if the control signal level (orange pin) falls within the range specified in the numerical spin controls (>) and (<). | + | [[resources/tools-software/sigmastudio/toolbox/multiplexersdemultiplexers|Click here to return to the Multiplexers/Demultiplexers page]] |
{{ :resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:statemachine024.jpg?|}} | {{ :resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:statemachine024.jpg?|}} | ||
+ | |||
+ | This block outputs the input signal from the green pin, if and only if the control signal level (orange pin) falls within the range specified in the numerical spin controls (>) and (<). | ||
If the control signal is out of range, the input is disabled and a zero value is output. | If the control signal is out of range, the input is disabled and a zero value is output. |