This is an old revision of the document!
Use the radio buttons in this multi-channel block to select among sets of 6 inputs and send one set to one of the (6-channel) outputs.
To begin, drag the block into the workspace, right-click it and select Add Algorithm > IC # > 6 Channel/Slew or 6 Channel. (The result, shown at right top, appears the same either way.)
The 6 Channel/Slew algorithm lets you rapidly ramp the source level up and down without any clicking noises when switching among outputs. It uses N hardware volume controls in the target/slew RAM to do the job.
The default block (shown at right) is ready to use as a 2×1 connection, and like the others can be grown by right-clicking to select your desired number of input sets. Shown at lower right is the default grown by 3 (= 5 input sets total).