This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:multichswitchnx6 [03 Aug 2012 17:17] – Created Brett Gildersleeve | resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:multichswitchnx6 [03 Aug 2012 17:37] (current) – Added link Brett Gildersleeve | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Multi-channel Switch Nx6 ====== | ====== Multi-channel Switch Nx6 ====== | ||
- | Use the radio buttons in this multi-channel block to select among sets of 6 inputs and send one set to one of the (6-channel) outputs. | + | [[resources/ |
{{ : | {{ : | ||
+ | |||
+ | Use the radio buttons in this multi-channel block to select among sets of 6 inputs and send one set to one of the (6-channel) outputs. | ||
To begin, drag the block into the workspace, right-click it and select Add Algorithm > IC # > 6 Channel/ | To begin, drag the block into the workspace, right-click it and select Add Algorithm > IC # > 6 Channel/ |