This shows you the differences between two versions of the page.
Last revisionBoth sides next revision | |||
resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:multichswitchnx4 [21 Jun 2012 22:36] – created Brett Gildersleeve | resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:multichswitchnx4 [03 Aug 2012 17:18] – Created Brett Gildersleeve | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | <WRAP center round todo 60%> | + | ====== Multi-channel Switch Nx4 ====== |
- | Under Construction | + | |
- | </ | + | |
+ | Use the radio buttons in this multichannel block to select among sets of 4 inputs and send one set to one of the (4-channel) outputs. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | To begin, drag the block into the workspace, right-click it and select Add Algorithm > IC # > 4 Channel/ | ||
+ | |||
+ | The default block (above right) is ready to use as a 2x1 connection, and like the others can be grown by right-clicking to select your desired number of input sets. The example to the right shows the default block grown by 3 (= 5 input sets total). |