This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:monoswitch1xn [03 Aug 2012 17:21] – Created Brett Gildersleeve | resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:monoswitch1xn [03 Aug 2012 17:38] (current) – Added link Brett Gildersleeve | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Mono Switch 1xN ====== | ====== Mono Switch 1xN ====== | ||
- | The Mono Switch block routes an input signal | + | [[resources/ |
{{ : | {{ : | ||
+ | |||
+ | The Mono Switch block routes an input signal to one of many possible outputs, the strip of radio buttons is used to select an output (each radio button corresponds to a coefficient RAM parameter). | ||
To begin, drag the block into the workspace, right-click it and select Add Algorithm > IC N Mono/Slew or Mono. (The result appears the same.) The Mono/Slew algorithm lets you rapidly ramp the source level up and down without any clicking noises when switching outputs. It uses N hardware volume controls in the target/slew RAM to do its job. | To begin, drag the block into the workspace, right-click it and select Add Algorithm > IC N Mono/Slew or Mono. (The result appears the same.) The Mono/Slew algorithm lets you rapidly ramp the source level up and down without any clicking noises when switching outputs. It uses N hardware volume controls in the target/slew RAM to do its job. |