Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:monoswitch1xn [03 Aug 2012 17:21]
Brett Gildersleeve Created
resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:monoswitch1xn [03 Aug 2012 17:38]
Brett Gildersleeve Added link
Line 1: Line 1:
 ====== Mono Switch 1xN ====== ====== Mono Switch 1xN ======
  
-The Mono Switch block routes an input signal ​to one of many possible outputs, ​the strip of radio buttons is used to select an output (each radio button corresponds to a coefficient RAM parameter).+[[resources/​tools-software/​sigmastudio/​toolbox/​multiplexersdemultiplexers|Click here to return ​to the Multiplexers/​Demultiplexers page]]
  
 {{ :​resources:​tools-software:​sigmastudio:​toolbox:​multiplexersdemultiplexers:​multichannelswitch1xn_032.jpg?​|}} {{ :​resources:​tools-software:​sigmastudio:​toolbox:​multiplexersdemultiplexers:​multichannelswitch1xn_032.jpg?​|}}
 +
 +The Mono Switch block routes an input signal to one of many possible outputs, the strip of radio buttons is used to select an output (each radio button corresponds to a coefficient RAM parameter).
  
 To begin, drag the block into the workspace, right-click it and select Add Algorithm > IC N Mono/Slew or Mono. (The result appears the same.) The Mono/Slew algorithm lets you rapidly ramp the source level up and down without any clicking noises when switching outputs. It uses N hardware volume controls in the target/slew RAM to do its job. To begin, drag the block into the workspace, right-click it and select Add Algorithm > IC N Mono/Slew or Mono. (The result appears the same.) The Mono/Slew algorithm lets you rapidly ramp the source level up and down without any clicking noises when switching outputs. It uses N hardware volume controls in the target/slew RAM to do its job.
resources/tools-software/sigmastudio/toolbox/multiplexersdemultiplexers/monoswitch1xn.txt · Last modified: 03 Aug 2012 17:38 by Brett Gildersleeve