This shows you the differences between two versions of the page.
Previous revisionNext revision | |||
— | resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:crossfadedatacontrolled [03 Aug 2012 17:39] – Added link Brett Gildersleeve | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== Crossfade (Data-Controlled) ====== | ||
+ | [[resources/ | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | This block creates a smooth transition between two input signals: the volume of one signal is decreased while the other input signal level increases, creating a gradual switch (cross-fade) between the inputs. | ||
+ | |||
+ | The output signal is selected by setting a value on the input control pin (top orange pin) to the desired input' | ||
+ | |||
+ | When the control input value changes, a cross fade is initiated between the current output and the newly selected input signal. The cross-fade transition rate (slew rate) can be adjusted using the numerical control on the block, (the maximum SW Slew Rate value is 23). | ||
+ | |||
+ | This block' | ||
+ | |||
+ | * Select Grow Algorithm from the right-click menu to create an additional output and input pair (sharing the signal select control pin and SW slew ram parameter). | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | * Select Add Algorithm from the right-click menu to create an additional algorithm with its own independent input select control pin. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | See the Multiplexer/ |