Wiki

no way to compare when less than two revisions

Differences

This shows you the differences between two versions of the page.


Previous revision
Next revision
resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:crossfadedatacontrolled [03 Aug 2012 17:39] – Added link Brett Gildersleeve
Line 1: Line 1:
 +====== Crossfade (Data-Controlled) ======
  
 +[[resources/tools-software/sigmastudio/toolbox/multiplexersdemultiplexers|Click here to return to the Multiplexers/Demultiplexers page]]
 +
 +{{ :resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:crossfadedatacontrolled042.jpg?|}}
 +
 +This block creates a smooth transition between two input signals: the volume of one signal is decreased while the other input signal level increases, creating a gradual switch (cross-fade) between the inputs.
 +
 +The output signal is selected by setting a value on the input control pin (top orange pin) to the desired input's index of either 0.0 or 1.0. The control signal should be a 28.0 format integer value, typically from a  DC input block or RMS Table.
 +
 +When the control input value changes, a cross fade is initiated between the current output and the newly selected input signal. The cross-fade transition rate (slew rate) can be adjusted using the numerical control on the block, (the maximum SW Slew Rate value is 23).
 +
 +This block's algorithm can be grown or added:
 +
 +  * Select Grow Algorithm from the right-click menu to create an additional output and input pair (sharing the signal select control pin and SW slew ram parameter).
 +
 +{{ :resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:crossfadedatacontrolled043.jpg? |}}
 +
 +  * Select Add Algorithm from the right-click menu to create an additional algorithm with its own independent input select control pin.
 +
 +{{ :resources:tools-software:sigmastudio:toolbox:multiplexersdemultiplexers:crossfadedatacontrolled044.jpg? |}}
 +
 +See the Multiplexer/Demultiplexer Example of the Crossfade (Data-Controlled) block.
resources/tools-software/sigmastudio/toolbox/multiplexersdemultiplexers/crossfadedatacontrolled.txt · Last modified: 17 Jun 2014 23:59 by Jonathan Bright