Wiki

This version (03 Aug 2012 17:54) was approved by Brett Gildersleeve.

Multiple-Control Splitter

Click here to return to the Mixers/Splitters page

The Multiple Control Splitter allows an input signal to be split into two or more outputs with independent control of each output's gain settings

There is a control knob for setting the gain or each output. To set the gain, click the knob with the left mouse button and drag while holding down the button. Each knob's range, value, and step size can be customized in the control pop-up window. To change the knob settings, right-click on the knob control.

The block can be grown by right-clicking and selecting Grow Algorithm from the menu. Growing creates additional output pins and control knob. Up to 15 outputs maximum can be created (13 more than the initial 2 outputs).

resources/tools-software/sigmastudio/toolbox/mixerssplitters/multiplecontrolsplitter.txt · Last modified: 03 Aug 2012 17:54 by Brett Gildersleeve