Wiki

This version (03 Aug 2012 17:56) was approved by Brett Gildersleeve.The Previously approved version (03 Aug 2012 17:53) is available.Diff

Multiple-Control Mixer

Click here to return to the Mixers/Splitters page

The Multiple Control Mixer allows a set of input signals to be mixed, with variable gain, into a single output signal. The Multiple-Control Mixer is similar to the Cross-Mixer blocks, however this block has a different Grow behavior. Growing this block will increase the number of inputs while growing a cross mixer block increases the number of outputs.

Adding Additional Inputs

Right-click, select Grow Algorithm from the menu, and choose the number of input pins to add. By default this block will have two input pins.

resources/tools-software/sigmastudio/toolbox/mixerssplitters/multiplecontrolmixer.txt · Last modified: 03 Aug 2012 17:56 by Brett Gildersleeve