Wiki

This version is outdated by a newer approved version.DiffThis version (17 Sep 2016 10:00) was approved by Venkatesan Krishnamoorthy.The Previously approved version (29 Aug 2016 08:02) is available.Diff

This is an old revision of the document!


Audio Signal Router Index Selectable

Click here to return to the Mixers/Splitters page

Audio Signal router mixes M different inputs to N different outputs with various gains. The number of input and output pins are configurable.

Configuration

This module supports multiple mixer configurations. Each mixer configuration has gains for all the inputs and outputs. A separate gain is available for each of input output combination also. All the gains has a corresponding mute control to quickly mute the particular gain. The current mixer (Mix #) can be changed during the runtime.

The following equations show the calculation of the output for given sample mixer table.

Out0 Out1
Og0 Og1
In0 Ig0 G00 G01
In1 Ig1 G10 G11
  1. Out0 = Og0 * ( G00 * Ig0 * In0 + G10 * Ig1 * In1)
  2. Out1 = Og1 * ( G01 * Ig0 * In0 + G11 * Ig1 * In1)

If the input/output channels are more than 16, then the mixer window is split for 16 input/output channels to improve GUI performance.

Labels for each of the input/output channels can be edited. This updated channel name will pear on the each of the Pin's tooltip as show below.



DSP Parameter Information

Compiler NameFunction Description
InputGain_t_iGain for the Mix t and Input i.
OutputGain_t_jGain for the Mix t and Output j.
CrossGain_t_j_iCrossGain for the Mix t, Output j and Input i.
TabIndex Current Mix to apply

Note:Here t,i and j starts from 0.
All the parameter names are appended with the algorithm name (e.g.)AudioSignalRouterIndxSel32S300Alg1InputGain_0_0

resources/tools-software/sigmastudio/toolbox/mixerssplitters/audiosignalrouterindexselectable.1474093635.txt.gz · Last modified: 17 Sep 2016 08:27 by Venkatesan Krishnamoorthy