Click here to return to the miscelleneous page
PCM to PCMx conversion will have a control signal, which will carry the header information
required by the PCMx signal, and 2 Data (PCM) pins, each carrying Linear PCM data, of size
Schematic Block Size, as input. The output is PCMx format which will have 3 * Schematic Block
Size no of samples. PCM to PCMx does the reverse of PCMx to PCM module.
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Input1 | decimal - Control | Control signal with header information for the PCMx signal |
Pin 1: Input2 | decimal - PCM data | Linear PCM data of Block size |
Pin 2: Input3 | decimal - PCM data | Linear PCM data of Block size |
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Output | decimal- PCMx | PCMx input of size 2* Block Size PCM data and 1* Block Size of header info |
The module does not support Add. The module supports growth. When grown to a growth count of 'r' the number of samples in each PCM input is given by (2* block size)/r.
GUI Control Name | Compiler Name | Function Description |
---|---|---|
- | - | - |
PCM to PCMx conversion will have a control signal, which will carry the header information
required by the PCMx signal, and 2 Data (PCM) pins, each carrying Linear PCM data, of size
Schematic Block Size, as input. The output is PCMx format which will have 3 * Schematic Block
Size no of samples.