Wiki

This version is outdated by a newer approved version.DiffThis version (15 May 2018 12:42) was approved by Sanjeeva Reddy.The Previously approved version (30 Jun 2017 10:38) is available.Diff

This is an old revision of the document!


Master Control Port (ADAU145X)

Click here to return to the Toolbox page

The Master Control Port library in the ToolBox lists blocks that utilize the ADAU145x processor family's master control port. These devices contain a combined I2C and SPI bus port accessible from a DSP program.

The master control port can be used for several purposes, as follows:

  • Self boot the ADAU145x processor from an external serial EEPROM.
  • Boot and control external slave devices such as codecs and amplifiers.
  • Read from and write to an external SPI RAM or flash memory.
  • Monitoring external I2C slaves during runtime
  • Reading a wav file from SPI flash and playing
  • Monitoring external SPI slaves during runtime

The following blocks are available:

resources/tools-software/sigmastudio/toolbox/mastercontrolport.1526380953.txt.gz · Last modified: 15 May 2018 12:42 by Sanjeeva Reddy