This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:tools-software:sigmastudio:toolbox:mastercontrolport:mastercontrolportstatus [26 Apr 2016 06:28] – created Venkatesan Krishnamoorthy | resources:tools-software:sigmastudio:toolbox:mastercontrolport:mastercontrolportstatus [31 Aug 2016 07:25] (current) – Venkatesan Krishnamoorthy | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Master Control Port Runtime Sequential Write (ADAU145x) ====== | + | ====== Master Control Port Status |
[[resources: | [[resources: | ||
Line 6: | Line 6: | ||
\\ | \\ | ||
- | The master control port Status block sends out the Master control port status in the output pin. | + | The master control port Status block sends out the Master control port status in the output |
+ | ===Input Pins=== | ||
+ | ^Name^Format [int/dec] - [control/ | ||
+ | |Pin 0: Master Control Port Error Clear|decimal - control|Any non -zero value in the input clears the error.| | ||
===Output Pins=== | ===Output Pins=== | ||
^Name^Format [int/dec] - [control/ | ^Name^Format [int/dec] - [control/ | ||
|Pin 0: Master Control Port Status|decimal - control|Outputs 1 while the Master control port is busy, otherwise outputs 0| | |Pin 0: Master Control Port Status|decimal - control|Outputs 1 while the Master control port is busy, otherwise outputs 0| | ||
+ | |Pin 1: Master Control Port Error|decimal - control|It is a 2 bit value. Bit-0 is set if I2C error is encountered. Bit-1 is set when timeout error occurred. | | ||