Click here to return to the Master Control Port page
The master control port Runtime Sequential Write block allows communication with external devices during audio processing. Typically this block is used to transfer data to an external device like a converter or codec. Communication over the master control port bus (I2C or SPI) occurs once per external trigger. The data transferred between host and device is defined in a SigmaStudio sequence file which can be generated using the SigmaStudio sequence window.
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Trigger | decimal - control | Rising edge in the trigger signal, initiates the sequential write |
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Write Status | decimal - control | Outputs 1 while the sequential write is in progress. otherwise outputs 0 |
Click on to configure the parameters.
GUI Control Name | Default Value | Range | Function Description |
---|---|---|---|
Bitrate | 400 kHz | 20 kHZ - 400 kHZ | I2C Speed |
Device Address | 0 | 0 – 127 | I2C Slave Device Address |
Sub-Address Bytes | 2 | 1-4 | Length of the sub address |
Sequence file | - | - | Device write/read sequence to execute at boot time.This file can be defined and saved from SigmaStudio's sequence window. |
GUI Control Name | Default Value | Range | Function Description |
---|---|---|---|
Bitrate | 100 kHz | 100 kHZ - 100000 kHZ | SPI Speed |
SS_M Pin | 0 | 0 | SPI Slave Select |
MP Slave Select Channel | Disabled (Enabled by click on radio button) | 0 – 7 | SPI Slave Select Channel |
Sub-Address Bytes | 2 | 1-4 | Length of the sub address |
Command Length | 1 | 1-4 | Length of the command sent in bytes |
Write Instruction | 0 | 0-255 | Instruction value for a write operation (0x0 for ADI audio devices, typically 0x2 for eeprom/flash) |
Write-Enable instruction | 6 | 0 - 255 | Instruction value for device write-enable operation (ignored for Master Control Port I/O Boot) |
Multiple external devices can be configured by creating multiple instances of the Runtime Sequential Write module and selecting appropriate slave select pins in the configuration parameters as detailed below.
If the device to be programmed is selected through MP0 (the /SS_M pin), no configuration is required in the register controls. Otherwise, the multipurpose pin must be configured to act as the slave select in the Register Window. (Hardware Configuration → ICx - ADAU145x Register Controls → MULTIPURPOSE/AUXADC)
The following table shows the mapping between the module's parameter and the register control window. Please note that for some other blocks, there is an offset of 1 between the module parameter and the register control window.
'Slave Select' in Configuration Window | 'Slave Select Channel' in the Register Control Window |
---|---|
0 | Slave Select Channel 0 |
1 | Slave Select Channel 1 |
2 | Slave Select Channel 2 |
3 | Slave Select Channel 3 |
4 | Slave Select Channel 4 |
5 | Slave Select Channel 5 |
Use the following file and edit for your slave.
<?xml version="1.0" standalone="no"?> <ROM IC="ADAU1361" IC_Address="112" Address_byte_length="2"> <dateTime>2017-03-16T05:12:14.2859851Z</dateTime> <version>3.14.1.1593</version> <page modetype="Mode 0"> <action instr="writeXbytes" len="3" addr="16384" ParamName="Reg1" DspName="IC 1">0F</action> <action instr="writeXbytes" len="8" addr="16386" ParamName="Reg2" DspName="IC 1">00 FD 00 0C 20 01</action> <action instr="delay" ParamName="IC 1.Delay" DspName="IC 1">00 64</action> <action instr="writeXbytes" len="3" addr="16405" ParamName="IC 1.Serial Port Control Registers.Serial Port Control 0" DspName="IC 1">00</action> </page> </ROM>
Please follow the steps below to edit the XML for your Slave.
<ROM IC="ADAU1361" IC_Address="112" Address_byte_length="2">
<action instr="writeXbytes" len="8" addr="16386" ParamName="Reg2" DspName="IC 1">00 FD 00 0C 20 01</action>
Please match all the fields as follows. instr => "writeXBytes" len => Data Length in bytes+ Address_byte_length addr => Register Address in decimal (not hexadecimal) Then the value part should have the register values in Hexadecimal. A space should separate each data as shown in the example. In this example len => 6 (data length) + 2 (Address_byte_length) = 8
<action instr="delay" ParamName="IC 1.Delay" DspName="IC 1">00 64</action>
Delay is in milliseconds (Hexadecimal Format)