Wiki

This version (01 Dec 2014 20:23) was approved by John McCarty.The Previously approved version (03 Aug 2012 22:51) is available.Diff

Subharmonic Synth (LF)

Click here to return to the Licensed Algorithms page

This block is not included in the SigmaStudio installation. Please contact Analog Devices for evaluation and licensing information.

The Subharmonic Synth (low freq) cell is a synthesizer processor which produces and adds deep, typically near-infrasonic bass to the original audio signal.

Unlike an equalizer, which indiscriminately boosts bass that may be loud enough already, this cell automatically and intelligently creates new harmonics at half the frequency of the fundamentals present in the signal. The deep bass generated by this call is mixed with the regular audio to produce clear but significantly bass-enhanced sound.

Max Harmonic. Enter the maximum desired frequency of the subharmonic in the text field (or click and hold the up/down arrow), 40-120 Hz.

resources/tools-software/sigmastudio/toolbox/licensedalgorithms/subharmonicsynthlf.txt · Last modified: 01 Dec 2014 20:23 by John McCarty