Wiki

This version is outdated by a newer approved version.DiffThis version (06 Aug 2012 22:14) was approved by Brett Gildersleeve.

This is an old revision of the document!


Single Level Detector

Click here to return to the Level Detectors/Lookup Tables page

The Level Detector blocks calculate the input signal level, reading directly from the hardware in real time, and display the level graphically in meter displays. The Single-Level Detector calculates and displays the rms level of the signal, shown in dB.

The level detector performs analysis only and does not modify the input signal. The signal at the output pin is identical to the input.

Use the On / Off button to enable or disable the display. The level detector will not function until the schematic design has been compiled and downloaded to the hardware and a USB communication channel is properly configured.

The refresh rate of the display is approximately 10 Hz, while the green cross-bar tracks the maximum rms value with a slight delay. Note that the display's performance is limited by your PC system and USB communication resources. Using multiple level detectors may degrade the responsiveness.

resources/tools-software/sigmastudio/toolbox/leveldetectorslookuptables/singleleveldetector.1344284096.txt.gz · Last modified: 06 Aug 2012 22:14 by Brett Gildersleeve