This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:sigmastudio:toolbox:leveldetectorslookuptables:singleleveldetector [06 Aug 2012 22:14] – created Brett Gildersleeve | resources:tools-software:sigmastudio:toolbox:leveldetectorslookuptables:singleleveldetector [28 Jul 2020 15:32] (current) – Redirected to up-to-date page Joshua Berlin | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Single Level Detector ====== | + | ~~GOTO> |
- | [[resources: | ||
- | |||
- | {{ : | ||
- | |||
- | The Level Detector blocks calculate the input signal level, reading directly from the hardware in real time, and display the level graphically in meter displays. The Single-Level Detector calculates and displays the rms level of the signal, shown in dB. | ||
- | |||
- | The level detector performs analysis only and does not modify the input signal. The signal at the output pin is identical to the input. | ||
- | |||
- | Use the On / Off button to enable or disable the display. The level detector will not function until the schematic design has been compiled and downloaded to the hardware and a USB communication channel is properly configured. | ||
- | |||
- | The refresh rate of the display is approximately 10 Hz, while the green cross-bar tracks the maximum rms value with a slight delay. Note that the display' |