This shows you the differences between two versions of the page.
resources:tools-software:sigmastudio:toolbox:io:spdifinputoutput [21 Jun 2012 21:04] – created Brett Gildersleeve | resources:tools-software:sigmastudio:toolbox:io:spdifinputoutput [06 Aug 2012 22:45] (current) – created Brett Gildersleeve | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | <WRAP center round todo 60%> | + | ====== SPDIF Input/Output ====== |
- | Under Construction | + | |
- | </WRAP> | + | |
+ | [[resources: | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | The SPDIF Input and Output blocks route signals between the schematic design and the hardwares' | ||
+ | |||
+ | Use the input block' | ||
+ | |||
+ | Every enabled input must be connected to an output, else there will be errors on compilation. | ||
+ | |||
+ | To change the SPDIF Input block' | ||
+ | |||
+ | <WRAP center round info 60%> | ||
+ | Note: These blocks are only available for use with DSPs that have SPDIF I/O. | ||
+ | </ |