This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:sigmastudio:toolbox:io:inferfaceread1 [13 Sep 2016 21:58] – Mazher Khan | resources:tools-software:sigmastudio:toolbox:io:inferfaceread1 [13 Sep 2016 21:59] (current) – Mazher Khan | ||
---|---|---|---|
Line 12: | Line 12: | ||
- The current release has only the I2C features, SPI will be supported in the upcoming releases.\\ | - The current release has only the I2C features, SPI will be supported in the upcoming releases.\\ | ||
====Use Case==== | ====Use Case==== | ||
- | {{ : | + | {{ : |
The interface read module can be used an input moudule to the UPDown LUT. The Interface read module serves as a starting index to the UPDown LUT. One of the outputs of the UPDown LUT module is given to the Interface write module which will write the same to the EEPROM. | The interface read module can be used an input moudule to the UPDown LUT. The Interface read module serves as a starting index to the UPDown LUT. One of the outputs of the UPDown LUT module is given to the Interface write module which will write the same to the EEPROM. | ||