Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:tools-software:sigmastudio:toolbox:io:inferfaceread1 [13 Sep 2016 21:58]
Mazher Khan
resources:tools-software:sigmastudio:toolbox:io:inferfaceread1 [13 Sep 2016 21:59]
Mazher Khan
Line 12: Line 12:
    - The current release has only the I2C features, SPI will be supported in the upcoming releases.\\    - The current release has only the I2C features, SPI will be supported in the upcoming releases.\\
 ====Use Case==== ====Use Case====
-{{ :​resources:​tools-software:​sigmastudio:​toolbox:​io:​usecaseinterfacereadandwrite.png?nolink |}}+{{ :​resources:​tools-software:​sigmastudio:​toolbox:​io:​usecase1.png?nolink |}}
  
 The interface read module can be used an input moudule to the UPDown LUT. The Interface read module serves as a starting index to the UPDown LUT. One of the outputs of the UPDown LUT module is given to the Interface write module which will write the same to the EEPROM. The interface read module can be used an input moudule to the UPDown LUT. The Interface read module serves as a starting index to the UPDown LUT. One of the outputs of the UPDown LUT module is given to the Interface write module which will write the same to the EEPROM.
  
  
resources/tools-software/sigmastudio/toolbox/io/inferfaceread1.txt · Last modified: 13 Sep 2016 21:59 by Mazher Khan