Wiki

This version (03 Aug 2012 23:05) was approved by William Jahn.

Toggle On/Off

Click here to return to the GPIO Conditioning page

The Toggle On/Off cell toggles its output when it detects a rising edge on its input. The amplitude of the output signal can be set using the drop-down control in the cell's GUI.

Input Pins

NameFormat
[int/dec] - [control/audio]
Function Description
Pin 0: Detection inputinteger or decimal - controlControl Signal input that is detected by the toggle on/off cell
Pin 1: Interface read inputother - interface registerConnected to a software interface register - reads the last stored value at startup

Output Pins

NameFormat
[int/dec] - [control/audio]
Function Description
Pin 0: Toggle outputinteger - controlToggling output. Toggles between zero and one each time a rising edge is detected on the input.
Pin 1: Interface write outputother - interface registerConnected to a software interface register - writes the last output value

GUI Controls

GUI Control NameDefault ValueRangeFunction Description
Drop-down menu2828.0, bits 1 to 22, 5.23, bits 24 to 26Controls which bit on the output signals will toggle on/off. For example, if this control is set to 28.0, then bit [0] will toggle on the output signal. If this control is set to 5.23, then bit [23] will toggle on the output signal. All other bits remain at zero at all times.

DSP Parameter Information

GUI NameCompiler NameFunction Description
Drop-down menuToggleOneAlg1output1Defines the bit that will be toggled on the output. In other words, the output will toggle between zero and this value. As an example, if the drop-down menu is set to “28.0”, then the value stored in RAM will be 0X00, 0X00, 0X00, 0X01, or one in 28.0 format.

Algorithm Description

The toggle on/off cell detects rising edges on its input and toggles its output each time another rising edge is encountered. In other words, if the output is zero and a rising edge appears on the input, the output will change to one. Conversely, if the output is one and a rising edge appears on the input, the output will change to zero. The graphic below shows this input to output relationship.



The output of the cell will always toggle between zero and another number. That number is determined by the value in the drop-down menu in the GUI. For example, in the above graphic, only the LSB was toggling, so the output was toggling between zero and one in integer format.

In the example below, the 23rd bit (in a SigmaDSP with 5.23 decimal representation) is toggling. Therefore, the output toggles between zero and 0.5 in decimal format.



The input to this cell should only take on two values - for example, a logic switch or a square wave. Signals such as sine waves or noise signals will cause the cell to behave in an unpredictable way.

Example

This simple example will toggle the 24th bit on the output each time the input switch outputs a rising edge. The output will be a series of zeros and ones in 5.23 format.



Other cells used in this example: On/Off Switch, Interface Read, Interface Write, Output

Algorithm Details

Toolbox PathGPIO Conditioning - PushButton - Toggle OnOff - Toggle OnOff
Cores SupportedADAU144x
ADAU1701
ADAU1761
ADAU1781
“Grow Algorithm” Supportedno
“Add Algorithm” Supportedno
Subroutine/Loop Basedno
Program RAM10
Data RAM4
Parameter RAM1
resources/tools-software/sigmastudio/toolbox/gpioconditioning/toggleonoff.txt · Last modified: 03 Aug 2012 23:05 by William Jahn