The information here is preliminary.
Click here to return to the SigmaStudio Algorithm Resource Summary section.
Category | Algorithm | Executed Instructions | Program RAM | DATA Ram | Parameter RAM | Description | Processors | ||
---|---|---|---|---|---|---|---|---|---|
Second Order | Single Precision | 2 Ch Optimized | General (2nd Order) | 17 | 17 | 14 | 9 | Gives access to a wide variety of 2nd-order (biquad) filter algorithms, including parametric, shelving, HP/LP/BP/BS, Butterworth, Bessel, tone, IIR coefficient, all pass, peaking, notch, and Chebyshev. If one of these cells is used in a project, one instance of the Biquad Looping SP subroutine is called. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 2 Ch Optimized | General (2nd Order) (Grow) | 0 | 0 | 6 | 5 | Adds another General (2nd Order) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. For each time the algorithm is grown, the Biquad Looping SP subroutine's resource usage increases by the amounts shown in the Biquad Looping SP (Grow) row. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 2 Ch Optimized | Medium Size EQ | 17 | 17 | 14 | 9 | Gives access to two general 2nd-order filters: Peaking and Shelving EQ. If one of these cells is used in a project, one instance of the Biquad Looping SP subroutine is called. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 2 Ch Optimized | Medium Size EQ (Grow) | 0 | 0 | 6 | 5 | Adds another Medium Sized filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. For each time the algorithm is grown, the Biquad Looping SP subroutine's resource usage increases by the amounts shown in the Biquad Looping SP (Grow) row.increases by the amounts shown in the Biquad Looping SP (Grow) row. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 2 Ch Optimized | Text-In (Unlinked) | 17 | 17 | 14 | 9 | Alternative to the General-Purpose filter, the Text-In block lets you set parameters using text fields, without having to open another window. If one of these cells is used in a project, one instance of the Biquad Looping SP subroutine is called. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 2 Ch Optimized | Text-In (Unlinked) (Grow) | 0 | 0 | 6 | 5 | Adds another Text-In (Unlinked) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. For each time the algorithm is grown, the Biquad Looping SP subroutine's resource usage increases by the amounts shown in the Biquad Looping SP (Grow) row. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 1 Ch Optimized | General (2nd Order) | 10 | 10 | 7 | 8 | Gives access to a wide variety of 2nd-order (biquad) filter algorithms, including parametric, shelving, HP/LP/BP/BS, Butterworth, Bessel, tone, IIR coefficient, all pass, peaking, notch, and Chebyshev. If one of these cells is used in a project, one instance of the Biquad Looping SP subroutine is called. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 1 Ch Optimized | General (2nd Order) (Grow) | 0 | 0 | 3 | 5 | Adds another General (2nd Order) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. For each time the algorithm is grown, the Biquad Looping SP subroutine's resource usage increases by the amounts shown in the Biquad Looping SP (Grow) row. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 1 Ch Optimized | Medium Size EQ | 10 | 10 | 7 | 8 | Gives access to two general 2nd-order filters: Peaking and Shelving EQ. If one of these cells is used in a project, one instance of the Biquad Looping SP subroutine is called. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 1 Ch Optimized | Medium Size EQ (Grow) | 0 | 0 | 3 | 5 | Adds another Medium Sized filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. For each time the algorithm is grown, the Biquad Looping SP subroutine's resource usage increases by the amounts shown in the Biquad Looping SP (Grow) row. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 1 Ch Optimized | Text-In (Unlinked) | 10 | 10 | 7 | 8 | Alternative to the General-Purpose filter, the Text-In block lets you set parameters using text fields, without having to open another window. If one of these cells is used in a project, one instance of the Biquad Looping SP subroutine is called. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 1 Ch Optimized | Text-In (Unlinked) (Grow) | 0 | 0 | 3 | 5 | Adds another Text-In (Unlinked) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. For each time the algorithm is grown, the Biquad Looping SP subroutine's resource usage increases by the amounts shown in the Biquad Looping SP (Grow) row. | ADAU144x, ADAU176x, ADAU1781 |
Subroutine | Biquad Looping SP | 13/ch | 13 | 0 | 0 | Subroutine for general 2nd order single precision optimized filter. | ADAU144x, ADAU176x, ADAU1781 | ||
Subroutine | Biquad Looping SP (Grow) | 6/ch | 0 | 0 | 0 | Additional resources used when above subroutine is grown. | ADAU144x, ADAU176x, ADAU1781 | ||
Second Order | Single Precision | 1 Ch | General (2nd Order) | 6 | 6 | 6 | 5 | Gives access to a wide variety of 2nd-order (biquad) filter algorithms, including parametric, shelving, HP/LP/BP/BS, Butterworth, Bessel, tone, IIR coefficient, all pass, peaking, notch, and Chebyshev. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 1 Ch | General (2nd Order) (Grow) | 6 | 6 | 3 | 5 | Adds another General (2nd Order) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 1 Ch | Medium Size EQ | 6 | 6 | 6 | 5 | Gives access to two general 2nd-order filters: Peaking and Shelving EQ. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 1 Ch | Medium Size EQ (Grow) | 6 | 6 | 3 | 5 | Adds another Medium Sized filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 1 Ch | Text-In (Unlinked) | 6 | 6 | 6 | 5 | Alternative to the General-Purpose filter, the Text-In block lets you set parameters using text fields, without having to open another window. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 1 Ch | Text-In (Unlinked) (Grow) | 6 | 6 | 3 | 5 | Adds another Text-In (Unlinked) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 2 Ch | General (2nd Order) | 12 | 12 | 12 | 5 | Gives access to a wide variety of 2nd-order (biquad) filter algorithms, including parametric, shelving, HP/LP/BP/BS, Butterworth, Bessel, tone, IIR coefficient, all pass, peaking, notch, and Chebyshev. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 2 Ch | General (2nd Order) (Grow) | 12 | 12 | 6 | 5 | Adds another General (2nd Order) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 2 Ch | Medium Size EQ | 12 | 12 | 12 | 5 | Gives access to two general 2nd-order filters: Peaking and Shelving EQ. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 2 Ch | Medium Size EQ (Grow) | 12 | 12 | 6 | 5 | Adds another Medium Sized filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 2 Ch | Text-In (Unlinked) | 12 | 12 | 12 | 5 | Alternative to the General-Purpose filter, the Text-In block lets you set parameters using text fields, without having to open another window. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 2 Ch | Text-In (Unlinked) (Grow) | 12 | 12 | 6 | 5 | Adds another Text-In (Unlinked) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 3 Ch | General (2nd Order) | 18 | 18 | 18 | 5 | Gives access to a wide variety of 2nd-order (biquad) filter algorithms, including parametric, shelving, HP/LP/BP/BS, Butterworth, Bessel, tone, IIR coefficient, all pass, peaking, notch, and Chebyshev. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 3 Ch | General (2nd Order) (Grow) | 18 | 18 | 9 | 5 | Adds another General (2nd Order) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 3 Ch | Medium Size EQ | 18 | 18 | 18 | 5 | Gives access to two general 2nd-order filters: Peaking and Shelving EQ. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 3 Ch | Medium Size EQ (Grow) | 18 | 18 | 9 | 5 | Adds another Medium Sized filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 3 Ch | Text-In (Unlinked) | 18 | 18 | 18 | 5 | Alternative to the General-Purpose filter, the Text-In block lets you set parameters using text fields, without having to open another window. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 3 Ch | Text-In (Unlinked) (Grow) | 18 | 18 | 9 | 5 | Adds another Text-In (Unlinked) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 4 Ch | General (2nd Order) | 24 | 24 | 24 | 5 | Gives access to a wide variety of 2nd-order (biquad) filter algorithms, including parametric, shelving, HP/LP/BP/BS, Butterworth, Bessel, tone, IIR coefficient, all pass, peaking, notch, and Chebyshev. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 4 Ch | General (2nd Order) (Grow) | 24 | 24 | 12 | 5 | Adds another General (2nd Order) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 4 Ch | Medium Size EQ | 24 | 24 | 24 | 5 | Gives access to two general 2nd-order filters: Peaking and Shelving EQ. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 4 Ch | Medium Size EQ (Grow) | 24 | 24 | 12 | 5 | Adds another Medium Sized filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 4 Ch | Text-In (Unlinked) | 24 | 24 | 24 | 5 | Alternative to the General-Purpose filter, the Text-In block lets you set parameters using text fields, without having to open another window. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 4 Ch | Text-In (Unlinked) (Grow) | 24 | 24 | 12 | 5 | Adds another Text-In (Unlinked) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 5 Ch | General (2nd Order) | 30 | 30 | 30 | 5 | Gives access to a wide variety of 2nd-order (biquad) filter algorithms, including parametric, shelving, HP/LP/BP/BS, Butterworth, Bessel, tone, IIR coefficient, all pass, peaking, notch, and Chebyshev. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 5 Ch | General (2nd Order) (Grow) | 30 | 30 | 15 | 5 | Adds another General (2nd Order) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 5 Ch | Medium Size EQ | 30 | 30 | 30 | 5 | Gives access to two general 2nd-order filters: Peaking and Shelving EQ. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 5 Ch | Medium Size EQ (Grow) | 30 | 30 | 15 | 5 | Adds another Medium Sized filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 5 Ch | Text-In (Unlinked) | 30 | 30 | 30 | 5 | Alternative to the General-Purpose filter, the Text-In block lets you set parameters using text fields, without having to open another window. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 5 Ch | Text-In (Unlinked) (Grow) | 30 | 30 | 15 | 5 | Adds another Text-In (Unlinked) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 6 Ch | General (2nd Order) | 36 | 36 | 36 | 5 | Gives access to a wide variety of 2nd-order (biquad) filter algorithms, including parametric, shelving, HP/LP/BP/BS, Butterworth, Bessel, tone, IIR coefficient, all pass, peaking, notch, and Chebyshev. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 6 Ch | General (2nd Order) (Grow) | 36 | 36 | 18 | 5 | Adds another General (2nd Order) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 6 Ch | Medium Size EQ | 36 | 36 | 36 | 5 | Gives access to two general 2nd-order filters: Peaking and Shelving EQ. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 6 Ch | Medium Size EQ (Grow) | 36 | 36 | 18 | 5 | Adds another Medium Sized filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 6 Ch | Text-In (Unlinked) | 36 | 36 | 36 | 5 | Alternative to the General-Purpose filter, the Text-In block lets you set parameters using text fields, without having to open another window. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 6 Ch | Text-In (Unlinked) (Grow) | 36 | 36 | 18 | 5 | Adds another Text-In (Unlinked) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 2 Ch Optimized | General (2nd Order) | 17 | 17 | 20 | 9 | Gives access to a wide variety of 2nd-order (biquad) filter algorithms, including parametric, shelving, HP/LP/BP/BS, Butterworth, Bessel, tone, IIR coefficient, all pass, peaking, notch, and Chebyshev. If one of these cells is used in a project, one instance of the Biquad Looping SP subroutine is called. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 2 Ch Optimized | General (2nd Order) (Grow) | 0 | 0 | 12 | 5 | Adds another General (2nd Order) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. For each time the algorithm is grown, the Biquad Looping SP subroutine's resource usage increases by the amounts shown in the Biquad Looping SP (Grow) row. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 2 Ch Optimized | Medium Size EQ | 17 | 17 | 20 | 9 | Gives access to two general 2nd-order filters: Peaking and Shelving EQ. If one of these cells is used in a project, one instance of the Biquad Looping SP subroutine is called. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 2 Ch Optimized | Medium Size EQ (Grow) | 0 | 0 | 12 | 5 | Adds another Medium Sized filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. For each time the algorithm is grown, the Biquad Looping SP subroutine's resource usage increases by the amounts shown in the Biquad Looping SP (Grow) row. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 2 Ch Optimized | Text-In (Unlinked) | 17 | 17 | 20 | 9 | Alternative to the General-Purpose filter, the Text-In block lets you set parameters using text fields, without having to open another window. If one of these cells is used in a project, one instance of the Biquad Looping SP subroutine is called. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 2 Ch Optimized | Text-In (Unlinked) (Grow) | 0 | 0 | 12 | 5 | Adds another Text-In (Unlinked) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. For each time the algorithm is grown, the Biquad Looping SP subroutine's resource usage increases by the amounts shown in the Biquad Looping SP (Grow) row. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 1 Ch Optimized | General (2nd Order) | 10 | 10 | 10 | 8 | Gives access to a wide variety of 2nd-order (biquad) filter algorithms, including parametric, shelving, HP/LP/BP/BS, Butterworth, Bessel, tone, IIR coefficient, all pass, peaking, notch, and Chebyshev. If one of these cells is used in a project, one instance of the Biquad Looping SP subroutine is called. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 1 Ch Optimized | General (2nd Order) (Grow) | 0 | 0 | 6 | 5 | Adds another General (2nd Order) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. For each time the algorithm is grown, the Biquad Looping SP subroutine's resource usage increases by the amounts shown in the Biquad Looping SP (Grow) row. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 1 Ch Optimized | Medium Size EQ | 10 | 10 | 10 | 8 | Gives access to two general 2nd-order filters: Peaking and Shelving EQ. If one of these cells is used in a project, one instance of the Biquad Looping SP subroutine is called. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 1 Ch Optimized | Medium Size EQ (Grow) | 0 | 0 | 6 | 5 | Adds another Medium Sized filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. For each time the algorithm is grown, the Biquad Looping SP subroutine's resource usage increases by the amounts shown in the Biquad Looping SP (Grow) row. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 1 Ch Optimized | Text-In (Unlinked) | 10 | 10 | 10 | 8 | Alternative to the General-Purpose filter, the Text-In block lets you set parameters using text fields, without having to open another window. If one of these cells is used in a project, one instance of the Biquad Looping SP subroutine is called. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 1 Ch Optimized | Text-In (Unlinked) (Grow) | 0 | 0 | 6 | 5 | Adds another Text-In (Unlinked) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. For each time the algorithm is grown, the Biquad Looping SP subroutine's resource usage increases by the amounts shown in the Biquad Looping SP (Grow) row. | ADAU144x, ADAU176x, ADAU1781 |
Subroutine | Biquad Looping SP | 13/ch | 13 | 0 | 0 | Subroutine for general 2nd order single precision optimized filter. | ADAU144x, ADAU176x, ADAU1781 | ||
Subroutine | Biquad Looping SP (Grow) | 6/ch | 0 | 0 | 0 | Additional resources used when above subroutine is grown. | ADAU144x, ADAU176x, ADAU1781 | ||
Second Order | Double Precision | 1 Ch | General (2nd Order) | 9 | 9 | 9 | 5 | Gives access to a wide variety of 2nd-order (biquad) filter algorithms, including parametric, shelving, HP/LP/BP/BS, Butterworth, Bessel, tone, IIR coefficient, all pass, peaking, notch, and Chebyshev. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 1 Ch | General (2nd Order) (Grow) | 9 | 9 | 6 | 5 | Adds another General (2nd Order) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 1 Ch | Medium Size EQ | 9 | 9 | 9 | 5 | Gives access to two general 2nd-order filters: Peaking and Shelving EQ. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 1 Ch | Medium Size EQ (Grow) | 9 | 9 | 6 | 5 | Adds another Medium Sized filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 1 Ch | Text-In (Unlinked) | 9 | 9 | 9 | 5 | Alternative to the General-Purpose filter, the Text-In block lets you set parameters using text fields, without having to open another window. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 1 Ch | Text-In (Unlinked) (Grow) | 9 | 9 | 6 | 5 | Adds another Text-In (Unlinked) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 2 Ch | General (2nd Order) | 18 | 18 | 18 | 5 | Gives access to a wide variety of 2nd-order (biquad) filter algorithms, including parametric, shelving, HP/LP/BP/BS, Butterworth, Bessel, tone, IIR coefficient, all pass, peaking, notch, and Chebyshev. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 2 Ch | General (2nd Order) (Grow) | 18 | 18 | 12 | 5 | Adds another General (2nd Order) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 2 Ch | Medium Size EQ | 18 | 18 | 18 | 5 | Gives access to two general 2nd-order filters: Peaking and Shelving EQ. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 2 Ch | Medium Size EQ (Grow) | 18 | 18 | 12 | 5 | Adds another Medium Sized filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 2 Ch | Text-In (Unlinked) | 18 | 18 | 18 | 5 | Alternative to the General-Purpose filter, the Text-In block lets you set parameters using text fields, without having to open another window. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 2 Ch | Text-In (Unlinked) (Grow) | 18 | 18 | 12 | 5 | Adds another Text-In (Unlinked) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 3 Ch | General (2nd Order) | 27 | 27 | 27 | 5 | Gives access to a wide variety of 2nd-order (biquad) filter algorithms, including parametric, shelving, HP/LP/BP/BS, Butterworth, Bessel, tone, IIR coefficient, all pass, peaking, notch, and Chebyshev. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 3 Ch | General (2nd Order) (Grow) | 27 | 27 | 18 | 5 | Adds another General (2nd Order) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 3 Ch | Medium Size EQ | 27 | 27 | 27 | 5 | Gives access to two general 2nd-order filters: Peaking and Shelving EQ. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 3 Ch | Medium Size EQ (Grow) | 27 | 27 | 18 | 5 | Adds another Medium Sized filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 3 Ch | Text-In (Unlinked) | 27 | 27 | 27 | 5 | Alternative to the General-Purpose filter, the Text-In block lets you set parameters using text fields, without having to open another window. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 3 Ch | Text-In (Unlinked) (Grow) | 27 | 27 | 18 | 5 | Adds another Text-In (Unlinked) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 4 Ch | General (2nd Order) | 36 | 36 | 36 | 5 | Gives access to a wide variety of 2nd-order (biquad) filter algorithms, including parametric, shelving, HP/LP/BP/BS, Butterworth, Bessel, tone, IIR coefficient, all pass, peaking, notch, and Chebyshev. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 4 Ch | General (2nd Order) (Grow) | 36 | 36 | 24 | 5 | Adds another General (2nd Order) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 4 Ch | Medium Size EQ | 36 | 36 | 36 | 5 | Gives access to two general 2nd-order filters: Peaking and Shelving EQ. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 4 Ch | Medium Size EQ (Grow) | 36 | 36 | 24 | 5 | Adds another Medium Sized filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 4 Ch | Text-In (Unlinked) | 36 | 36 | 36 | 5 | Alternative to the General-Purpose filter, the Text-In block lets you set parameters using text fields, without having to open another window. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 4 Ch | Text-In (Unlinked) (Grow) | 36 | 36 | 24 | 5 | Adds another Text-In (Unlinked) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 5 Ch | General (2nd Order) | 45 | 45 | 45 | 5 | Gives access to a wide variety of 2nd-order (biquad) filter algorithms, including parametric, shelving, HP/LP/BP/BS, Butterworth, Bessel, tone, IIR coefficient, all pass, peaking, notch, and Chebyshev. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 5 Ch | General (2nd Order) (Grow) | 45 | 45 | 30 | 5 | Adds another General (2nd Order) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 5 Ch | Medium Size EQ | 45 | 45 | 45 | 5 | Gives access to two general 2nd-order filters: Peaking and Shelving EQ. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 5 Ch | Medium Size EQ (Grow) | 45 | 45 | 30 | 5 | Adds another Medium Sized filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 5 Ch | Text-In (Unlinked) | 45 | 45 | 45 | 5 | Alternative to the General-Purpose filter, the Text-In block lets you set parameters using text fields, without having to open another window. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 5 Ch | Text-In (Unlinked) (Grow) | 45 | 45 | 30 | 5 | Adds another Text-In (Unlinked) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 6 Ch | General (2nd Order) | 54 | 54 | 54 | 5 | Gives access to a wide variety of 2nd-order (biquad) filter algorithms, including parametric, shelving, HP/LP/BP/BS, Butterworth, Bessel, tone, IIR coefficient, all pass, peaking, notch, and Chebyshev. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 6 Ch | General (2nd Order) (Grow) | 54 | 54 | 35 | 5 | Adds another General (2nd Order) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 6 Ch | Medium Size EQ | 54 | 54 | 54 | 5 | Gives access to two general 2nd-order filters: Peaking and Shelving EQ. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 6 Ch | Medium Size EQ (Grow) | 54 | 54 | 35 | 5 | Adds another Medium Sized filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 6 Ch | Text-In (Unlinked) | 54 | 54 | 54 | 5 | Alternative to the General-Purpose filter, the Text-In block lets you set parameters using text fields, without having to open another window. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 6 Ch | Text-In (Unlinked) (Grow) | 54 | 54 | 35 | 5 | Adds another Text-In (Unlinked) filter algorithm in series with the prior exisisting ones in the block. No new inputs or outputs. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | Parametric EQ | 9 | 9 | 9 | 5 | Extends the functionality of the General (2nd-Order) filter with an enhanced graphical filter design tool. | ADAU144x, ADAU176x, ADAU1781 | |
Second Order | Double Precision | General 2nd Order Index Selectable | 75 | 75 | 37 | 23 | Provides a wide variety of 2nd-order filter algorithms. This block extends the functionality of the General (2nd-Order / Lookup) filter with an enhanced graphical filter design tool. | ADAU144x, ADAU176x, ADAU1781 | |
Second Order | Double Precision | General 2nd Order Index Selectable (Grow) | 27 | 27 | 19 | 0 | Adds another channel to the block. | ADAU144x, ADAU176x, ADAU1781 | |
Second Order | Double Precision | General (2nd Order/Lookup) | 14 | 14 | 10 | 21 | Gives access to a wide variety of 2nd-order (biquad) filter algorithms, including parametric, shelving, HP/LP/BP/BS, Butterworth, Bessel, tone, IIR coefficient, all pass, peaking, notch, and Chebyshev. | ADAU144x, ADAU176x, ADAU1781 | |
Second Order | Double Precision | General (2nd Order/Lookup) (Grow) | 9 | 9 | 9 | 0 | Adds another channel to the block. | ADAU144x, ADAU176x, ADAU1781 | |
Second Order | Double Precision | 2 Ch | Idxselectable Indp. Multiple Band Filter | 22 | 22 | 20 | 11 | Allows for a data controlled index input to select a bank of filters for processing. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 2 Ch | Idxselectable Indp. Multiple Band Filter (Grow) | 0 | 0 | 0 | 7 | Adds a new row to the existing algorithm. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 1 Ch | Idxselectable Indp. Multiple Band Filter | 15 | 15 | 10 | 10 | Allows for a data controlled index input to select a bank of filters for processing. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | 1 Ch | Idxselectable Indp. Multiple Band Filter (Grow) | 0 | 0 | 0 | 7 | Adds a new row to the existing algorithm. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Double Precision | General 2nd Order W Var Param/Lookup/Slew | 75 | 75 | 37 | 23 | Gives access to a wide variety of 2nd-order (biquad) filter algorithms, including parametric, shelving, HP/LP/BP/BS, Butterworth, Bessel, tone, IIR coefficient, all pass, peaking, notch, and Chebyshev. | ADAU144x, ADAU176x, ADAU1781 | |
Second Order | Double Precision | General 2nd Order W Var P/L/S (Grow) | 27 | 27 | 19 | 0 | Adds another channel to the block. | ADAU144x, ADAU176x, ADAU1781 | |
Second Order | Single Precision | General 2nd Order Index Selectable | 69 | 69 | 31 | 23 | Provides a wide variety of 2nd-order filter algorithms. This block extends the functionality of the General (2nd-Order / Lookup) filter with an enhanced graphical filter design tool. | ADAU144x, ADAU176x, ADAU1781 | |
Second Order | Single Precision | General 2nd Order Index Selectable (Grow) | 21 | 21 | 13 | 0 | Adds another channel to the block. | ADAU144x, ADAU176x, ADAU1781 | |
Second Order | Single Precision | 2 Ch | Idxselectable Indp. Multiple Band Filter | 22 | 22 | 14 | 11 | Allows for a data controlled index input to select a bank of filters for processing. The number of rows of possible filters is determined by the “growth” of the algorithm. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 2 Ch | Idxselectable Indp. MBF (Grow) | 0 | 0 | 0 | 7 | Adds a new filter row to the existing algorithm. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 1 Ch | Idxselectable Indp. Multiple Band Filter | 15 | 15 | 7 | 10 | Allows for a data controlled index input to select a bank of filters for processing. The number of rows of possible filters is determined by the “growth” of the algorithm. | ADAU144x, ADAU176x, ADAU1781 |
Second Order | Single Precision | 1 Ch | Idxselectable Indp. MBF (Grow) | 0 | 0 | 0 | 7 | Adds a new filter row to the existing algorithm. | ADAU144x, ADAU176x, ADAU1781 |
Miscellaneous | State Variable (Q/F Input) | 13 | 13 | 5 | 0 | Allows for simultaneous access to three different filter types: lowpass, highpass, bandpass. | ADAU144x, ADAU176x, ADAU1781 | ||
Miscellaneous | Tracking Filter | 116 | 116 | 26 | 16 | Tracking Filters are useful for dynamic shifting of filtering. This particular tracking filter is a Peaking Filter algorithm. | ADAU144x, ADAU176x, ADAU1781 | ||
Miscellaneous | DC Blocking Filter | 6 | 6 | 7 | 1 | This filter is pre-configured, that is, it has set parameters for blocking direct-current components. | ADAU144x, ADAU176x, ADAU1781 | ||
Miscellaneous | De-Emphasis | 6 | 6 | 6 | 3 | Used to attenuate the high-frequency components boosted during recording with pre-emphasis. | ADAU144x, ADAU176x, ADAU1781 | ||
Miscellaneous | State Variable | 10 | 10 | 5 | 2 | Allows for simultaneous access to three different filter types: lowpass, highpass, and bandpass. | ADAU144x, ADAU176x, ADAU1781 | ||
Miscellaneous | State Variable (Q Input) | 11 | 11 | 5 | 1 | Allows for simultaneous access to three different filter types: lowpass, highpass, and bandpass. | ADAU144x, ADAU176x, ADAU1781 | ||
Miscellaneous | Pinking | 31 | 31 | 18 | 16 | Converts white noise, which is equal energy per hertz, to pink noise, which is equal energy per proportional or constant-percentage (e.g., logarithmic) band. | ADAU144x, ADAU176x, ADAU1781 | ||
Crossover | Single Precision | 2 Way | Crossover | 30 | 30 | 20 | 21 | Used in loudspeaker systems to split the audio signal into separate frequency bands. | ADAU144x, ADAU176x, ADAU1781 |
Crossover | Single Precision | 3 Way | Crossover | 57 | 57 | 36 | 42 | Used in loudspeaker systems to split the audio signal into separate frequency bands. | ADAU144x, ADAU176x, ADAU1781 |
Crossover | Double Precision | 2 Way | Crossover | 42 | 42 | 32 | 21 | Used in loudspeaker systems to split the audio signal into separate frequency bands. | ADAU144x, ADAU176x, ADAU1781 |
Crossover | Double Precision | 3 Way | Crossover | 81 | 81 | 60 | 42 | Used in loudspeaker systems to split the audio signal into separate frequency bands. | ADAU144x, ADAU176x, ADAU1781 |
First Order | First Order W Var Param/Lookup/Slew | 69 | 69 | 31 | 15 | Provides a selectable set of High-pass or Low-pass 1st-order filter responses with smooth (slew) transitions when selecting among responses. | ADAU144x, ADAU176x, ADAU1781 | ||
First Order | First Order W Var P/L/S (Grow) | 90 | 90 | 44 | 15 | Adds a corresponding input and output to the block. | ADAU144x, ADAU176x, ADAU1781 | ||
First Order | General (1st Order) | 6 | 6 | 6 | 3 | Allows you to design 1st-order lowpass and highpass filters. | ADAU144x, ADAU176x, ADAU1781 | ||
First Order | General (1st Order) (Grow) | 6 | 6 | 4 | 3 | Adds another General (1st Order) algorithm and controls in series with prior one(s) to the block. | ADAU144x, ADAU176x, ADAU1781 | ||
FIR | NLMS Filter | 111 | 111 | 268 | 297 | A normalized least mean-squares filter for use in echo cancelation. | ADAU144x, ADAU176x, ADAU1781 | ||
FIR | FIR Filter | 11 | 11 | 11 | 10 | Lets you design any FIR filter desired. | ADAU144x, ADAU176x, ADAU1781 |