This shows you the differences between two versions of the page.
resources:tools-software:sigmastudio:toolbox:filters:textinlinked [02 Aug 2012 16:25] William Jahn Added coneten from the help file |
resources:tools-software:sigmastudio:toolbox:filters:textinlinked [15 Nov 2012 17:24] William Jahn Fixed broken General 2nd-Order Filters link |
||
---|---|---|---|
Line 11: | Line 11: | ||
At right is an example of a default algorithm of 1ch - Double Precision grown by 1, with an added 2ch - Double Precision. The parameters are the same in the vertical settings because of the linked nature of this block; see below for more about that. | At right is an example of a default algorithm of 1ch - Double Precision grown by 1, with an added 2ch - Double Precision. The parameters are the same in the vertical settings because of the linked nature of this block; see below for more about that. | ||
- | See [[resources/tools-software/sigmastudio/algorithminformation/general2ndorderfilters|General 2nd-Order Algorithms]] for information about the algorithms driving these blocks. The available filters are: | + | See [[resources/tools-software/sigmastudio/toolbox/algorithminformation/general2ndorderfilters|General 2nd-Order Algorithms]] for information about the algorithms driving these blocks. The available filters are: |
Peaking EQ | Peaking EQ | ||
Shelving EQ: Low-/High-Shelf | Shelving EQ: Low-/High-Shelf |