This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:tools-software:sigmastudio:toolbox:filters:statevariableqinput [23 Jun 2020 21:50] Joshua Berlin Filter parameters now defined on a different page |
resources:tools-software:sigmastudio:toolbox:filters:statevariableqinput [23 Jun 2020 22:37] Joshua Berlin Fixed EngineerZone link |
||
---|---|---|---|
Line 10: | Line 10: | ||
As can be seen from the figure (above right), this block has two inputs and three outputs. The green (standard input) pin is for the signal and the orange is for a value to control filter Q. It's common to control the Q of the filter either by sending a [[resources/tools-software/sigmastudio/toolbox/sources/dcinputentry|DC input]] value to this pin or by using it with the RMS table to generate Q parameters from the input signal instead. | As can be seen from the figure (above right), this block has two inputs and three outputs. The green (standard input) pin is for the signal and the orange is for a value to control filter Q. It's common to control the Q of the filter either by sending a [[resources/tools-software/sigmastudio/toolbox/sources/dcinputentry|DC input]] value to this pin or by using it with the RMS table to generate Q parameters from the input signal instead. | ||
- | To have control over Q from a block parameter, refer to the [[resources/tools-software/sigmastudio/toolbox/filters/statevariable|State-Variable Filter]]. | + | To control Q from a block parameter, refer to the [[resources/tools-software/sigmastudio/toolbox/filters/statevariable|State-Variable Filter]]. |
The three output pins allows to choose among LP, HP, BP filters. This algorithm computes the coefficients for all filter types, giving simultaneous access. If your application does not require the use of all filter types, then the output may be connected to the [[resources/tools-software/sigmastudio/toolbox/systemschematicdesign/schematicterminal|terminal block]]. | The three output pins allows to choose among LP, HP, BP filters. This algorithm computes the coefficients for all filter types, giving simultaneous access. If your application does not require the use of all filter types, then the output may be connected to the [[resources/tools-software/sigmastudio/toolbox/systemschematicdesign/schematicterminal|terminal block]]. | ||
Set the center frequency in the Freq (Hz) field or by dragging the <--> arrows. | Set the center frequency in the Freq (Hz) field or by dragging the <--> arrows. | ||
- | |||
- | The format for Q is 5.23, and it is inverted. In other words... | + | The format for Q is 5.23 or 8.24 (depending on your processor), and it is inverted. In other words... |
- | Input to Q pin = 1/Q | + | Input to Q pin = <m>1/Q</m> |
- | http://ez.analog.com/message/41163#41163 | + | https://ez.analog.com/dsp/sigmadsp/f/q-a/66757/numeric-format-for-state-variable-q-f-input |