Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:tools-software:sigmastudio:toolbox:filters:pinking [15 Nov 2012 21:43]
William Jahn fixed pink filter and level detectors link
resources:tools-software:sigmastudio:toolbox:filters:pinking [23 Jun 2020 22:16]
Joshua Berlin Moved algorithm information to this page
Line 11: Line 11:
 The Pinking cell takes any input signal and outputs a signal with a 3dB drop per octave in linear terms. The Pinking cell takes any input signal and outputs a signal with a 3dB drop per octave in linear terms.
  
-See [[resources/​tools-software/​sigmastudio/​toolbox/​algorithmformation/​pinkfilter|Pink Filter Algorithm]] for information on the algorithm, and also look at the [[resources/​tools-software/​sigmastudio/​tutorials/​leveldetectorsexamples|Level Detectors Example]] to see the filter used in a schematic.+Navigate to the [[resources/​tools-software/​sigmastudio/​tutorials/​leveldetectorsexamples|Level Detectors Example]] to see the filter used in a schematic.
  
 After you have established your default algorithm, this cell can have algorithms added to it. If you're using more than one DSP board, you will need to add the initial algorithm for the desired board. In either case, right-click the cell and select **Add Algorithm > IC N > Pink Noise Filter** to add another set of input/​output pins. After you have established your default algorithm, this cell can have algorithms added to it. If you're using more than one DSP board, you will need to add the initial algorithm for the desired board. In either case, right-click the cell and select **Add Algorithm > IC N > Pink Noise Filter** to add another set of input/​output pins.
    
 +===== Algorithm Information =====
 +The Pinking Filter takes any broadband input and outputs a signal with a 3dB drop per octave. The classic use of this filter is to convert white noise (equal energy per hertz) to pink noise (equal energy per constant percentage, e.g., log bundling, as with an octave or subdivision).
  
- +To the human ear, which has an approximately logarithmic frequency response, white noise is distinctly trebly, while pink noise sounds broad and smooth, more like a waterfall. 
 + 
 +The graph below (generated using simulation stimulus and probe) shows the two responses of white (green line) and pink (red line) noise. But realize that while these graphs are displayed on the familiar audio log scale, the data have not been subjected to, that is, not integrated in, constant-percentage bundling, but remain in constant-frequency depiction. This is in contrast to the RTA-style graphs in example 8.1, Level Detectors / Lookup Tables, where both the data and the graph scale are logarithmic.
  
 +{{ :​resources:​tools-software:​sigmastudio:​toolbox:​filters:​pinkfilter1.png?​direct&​600 |}}
  
resources/tools-software/sigmastudio/toolbox/filters/pinking.txt · Last modified: 23 Jun 2020 22:16 by Joshua Berlin