Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:tools-software:sigmastudio:toolbox:filters:general2ndorderindexselectable [12 Jan 2017 09:50] – Venkatesan Krishnamoorthy | resources:tools-software:sigmastudio:toolbox:filters:general2ndorderindexselectable [23 Jun 2020 19:48] (current) – added note about sigma100 bug Joshua Berlin |
---|
| |
This block is implemented as a biquad filter that has multiple sets of coefficients stored in tables on the DSP. See [[resources/tools-software/sigmastudio/toolbox/algorithminformation/general2ndorderfilters|General 2nd-Order Filters]] (in Algorithm Information) for details about the biquad filter design techniques used for this block.\\ | This block is implemented as a biquad filter that has multiple sets of coefficients stored in tables on the DSP. See [[resources/tools-software/sigmastudio/toolbox/algorithminformation/general2ndorderfilters|General 2nd-Order Filters]] (in Algorithm Information) for details about the biquad filter design techniques used for this block.\\ |
| |
| <note important>As of SigmaStudio 4.5, Index Selectable Filters are not working on ADAU1701 or ADAU1401. The block is tested and working for ADAU176x, ADAU144x, ADAU145x, and ADAU146x.</note> |
| |
{{ :resources:tools-software:sigmastudio:toolbox:filters:general2ndindexpic2.jpg?nolink |}} | {{ :resources:tools-software:sigmastudio:toolbox:filters:general2ndindexpic2.jpg?nolink |}} |
|Load All|-|-|The ISF form also has a load all button. On clicking the Load all button the filter types of all added filters is changed to IIR Coefficient and enables loading of filter coefficient for all filters from a single text file containing the coefficients for all filters. | | |Load All|-|-|The ISF form also has a load all button. On clicking the Load all button the filter types of all added filters is changed to IIR Coefficient and enables loading of filter coefficient for all filters from a single text file containing the coefficients for all filters. | |
|Opacity|-|-|The "Opacity" control sets the transparency value of the control window| | |Opacity|-|-|The "Opacity" control sets the transparency value of the control window| |
|Slew|12|0-100|The "Slew Points" control sets how many transition points the algorithm uses to transition from one selected filter curve to another, increasing the number of points will provide smoother transitions| | |Slew|12|0-46/ 0-100|ADAU144x/ADAU176x supports upto 46 slew points.The "Slew Points" control sets how many transition points the algorithm uses to transition from one selected filter curve to another, increasing the number of points will provide smoother transitions| |
|Bypass|0|0 or 1|The "Bypass" check box disables the filter when checked| | |Bypass|0|0 or 1|The "Bypass" check box disables the filter when checked| |
|View|-|-|The "View" section only applies for the First Order filter type, this tool allows you to manage each first order filter and control its settings graphically. Refer to the Example for more details| | |View|-|-|The "View" section only applies for the First Order filter type, this tool allows you to manage each first order filter and control its settings graphically. Refer to the Example for more details| |