The IIR Elliptical Interpolated Lowpass Filter "Content should be added"
To module has spin text box to control the order of the filter.
Name | ADSP-214xx | ADSP-215xx/SC5xx | ADAU145x/146x |
---|---|---|---|
IIR Elliptical LowPass (Mono) | NA | B | NA |
IIR Elliptical LowPass (Stereo) | NA | B | NA |
Name | Type | Description |
---|---|---|
Pin0 | Audio | Input to the low pass filter |
Pin1 | Audio | Input to the low pass filter |
Name | Type | Description |
---|---|---|
Pin0 | Audio | filtered output |
Pin1 | Audio | filtered output |
GUI Parameter Name | Default Value | Range | Function Description |
---|---|---|---|
Order | 6 | 0 to 10 | Controls the order of the filter equation |
Parameter Name | Description | ADSP-214xx/SC5xx/215xx | ADAU145x/146x |
---|---|---|---|
Order | Order of the filter equations | Float | NA |
A0 | Filter coefficient A0 | Float | NA |
A1 | Filter coefficient A1 | Float | NA |
B0 | Filter coefficient B0 | Float | NA |
B1 | Filter coefficient B1 | Float | NA |
B2 | Filter coefficient B2 | Float | NA |