Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:tools-software:sigmastudio:toolbox:dynamicsprocessors:peaknogain [25 Jun 2012 17:00] – Approved William Jahnresources:tools-software:sigmastudio:toolbox:dynamicsprocessors:peaknogain [02 Jul 2013 23:29] (current) – gain *increases* after the signal drops Jonathan Bright
Line 11: Line 11:
 \\ \\
 ===Controls=== ===Controls===
-|Hold (ms)|{{peaknogainpic2.png}}|Controls the time (in ms) the compressor maintains its current output  gain setting before it starts decreasing as the input level decrease.| +|Hold (ms)|{{peaknogainpic2.png}}|Controls the time (in ms) the compressor maintains its current output gain setting after the input level decreases, before the gain starts increasing back to normal.| 
-|Decay (db/s)|{{peaknogainpic3.png}}|Controls the rate at which the compressor gain decreases in response to decrease in the input signal level, e.g. the "Release" time.|+|Decay (db/s)|{{peaknogainpic3.png}}|Controls the rate at which the compressor gain increases back to normal in response to decrease in the input signal level, e.g. the "Release" time.  Larger values result in faster recoveries.|
 |Soft Knee|{{peaknogainpic4.png}}|Soft-knee lets the compressor ease into action, making a less-abrupt change from unprocessed signal to compressed signal. Typically it sounds better. If it is not activated, the default is hard-knee behavior, meaning compression reduces signal level immediately when the threshold is passed.| |Soft Knee|{{peaknogainpic4.png}}|Soft-knee lets the compressor ease into action, making a less-abrupt change from unprocessed signal to compressed signal. Typically it sounds better. If it is not activated, the default is hard-knee behavior, meaning compression reduces signal level immediately when the threshold is passed.|
 |Show Graph|{{peaknogainpic5.png}}|Opens the Compression Curve editor window.| |Show Graph|{{peaknogainpic5.png}}|Opens the Compression Curve editor window.|
resources/tools-software/sigmastudio/toolbox/dynamicsprocessors/peaknogain.txt · Last modified: 02 Jul 2013 23:29 by Jonathan Bright