Wiki

This version is outdated by a newer approved version.DiffThis version (22 Jun 2012 23:03) was approved by William Jahn.

This is an old revision of the document!


Mono peak No Gain

Click here to return to the Dynamics Processors page


The Mono Peak (no gain) algorithm is a dynamics processor that can gate, expand, compress, and limit input signals. The detection path uses the peak level of the input signal to calculate the output gain. Hold and decay parameters are included to allow control of the output gain over time. The transfer function can be fully controlled (within the computational limits of the DSP) using the “Show Graph” GUI control.

Input Pins

NameFormat [int/dec] - [control/audio]Function Description
Pin 0: Audio Inputdecimal - audioAudio Input - Channel 0

Output Pins

NameFormat [int/dec] - [control/audio]Function Description
Pin 0: Audio Outputdecimal - audioAudio Output - Channel 0

GUI Controls

GUI Control NameDefault ValueRangeFunction Description
Hold (ms)00 to 2000Hold time applied to the output gain before it starts the decay ramp
Decay (dB/s)100 to 1000Speed of the linear decay ramp applied to the output gain until it reaches the current target output gain
Soft KneeDisabledEnabled or DisabledControls whether or not the corners (or “knees”) on the transfer function are smoothed or not
resources/tools-software/sigmastudio/toolbox/dynamicsprocessors/monopeaknogain.1340399007.txt.gz · Last modified: 22 Jun 2012 23:03 by William Jahn