This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:sigmastudio:toolbox:dynamicsprocessors:monopeaknogain [22 Jun 2012 23:03] – Added content (incomplete) William Jahn | resources:tools-software:sigmastudio:toolbox:dynamicsprocessors:monopeaknogain [25 Jun 2012 15:33] (current) – Approved William Jahn | ||
---|---|---|---|
Line 20: | Line 20: | ||
|Decay (dB/s)|10|0 to 1000|Speed of the linear decay ramp applied to the output gain until it reaches the current target output gain| | |Decay (dB/s)|10|0 to 1000|Speed of the linear decay ramp applied to the output gain until it reaches the current target output gain| | ||
|Soft Knee|Disabled|Enabled or Disabled|Controls whether or not the corners (or " | |Soft Knee|Disabled|Enabled or Disabled|Controls whether or not the corners (or " | ||
+ | |||
+ | ===DSP Parameter Information=== | ||
+ | ^GUI Name^Compiler Name^Function Description^ | ||
+ | |Show Graph|MonoChannelSingleDetectNoPost2prec1_1 \\ MonoChannelSingleDetectNoPost2prec1_p1_1 \\ MonoChannelSingleDetectNoPost2prec1_p1_1_autoincremented \\ ...|33 table points for input-to-output transfer function (compression curve)| | ||
+ | |Hold (ms)|MonoChannelSingleDetectNoPost2prec1hold_1|Sets the hold time of the compressor| | ||
+ | |Decay (dB/ | ||
+ | |||
+ | ===Example=== | ||
+ | This example shows the mono peak compressor being used on an analog input. Depending on the application, | ||
+ | \\ | ||
+ | {{monopeakpic2.png}}\\ | ||
+ | \\ | ||
+ | Other cells used in this example: Input, Output | ||
+ | |||
+ | ===Algorithm Details=== | ||
+ | |Toolbox Path|Dynamics Processors - Peak - Standard Resolution - Lower Range (-90 to +6 dB) - No Post Gain - Mono - Mono Peak (no gain)| | ||
+ | |Cores Supported|ADAU1781 \\ ADAU1761 \\ ADAU144x \\ ADAU170x \\ AD1940| | ||
+ | |"Grow Algorithm" | ||
+ | |"Add Algorithm" | ||
+ | |Subroutine/ | ||
+ | |Program RAM|41| | ||
+ | |Data RAM|13| | ||
+ | |Parameter RAM|35| | ||
+ | |||
+ | |||
+ | |||